请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM3488 我有一个相关的问题、
我将处理类似的应用(fsw=250kHz)、D=93%。
此 SEPIC 必须与外部时钟(50%)同步。 数据表中所说的 D 大于93%。
在满载(双轨@ 25mA)时使 LM3488同步并正常运行的权变措施是什么?
此致、
ELISA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.