请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ24075 BQ24075 IITERM 检测电流的最小分辨率是多少?
规格为0.1×ICHG (CE = LO、(EN1、EN2)≠(LO、LO))
如果 ICGH 设置为225mA、则电池完全检测点为22.5mA、它是否正确?
b 苏杰明
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.