大家好:
是否 建议使用合适的 LED 输出恒流驱动方案和 IC 器件型号?
应用:LED 驱动器;
输入电是三相电、工作时请从两相电气工作中选择一项;
参数:
额定 输入电压:277V~480Vac:
输出电压:42V;
输出功率:120W
模式:恒定电流输出
mos/二极管应力的电压是否不能超过650V? 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.