Other Parts Discussed in Thread: TPS92692
尊敬的先生/女士
我想针对9~12Vin 和15Vout/1A 升压拓扑修改 TPS92692EVM。
读取数据表后、是否正确修改了以下剂量?
R1格式0.3至0.1//01=0.05R。
J5连接 引脚1-2
J7连接引脚2-3
从29.4K 到26.1K。
我是对的吗?
此致、
黄上
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,Kami,
如果您阅读了数据表的第9.1.7节(第31页)。 ILED = VIADD/(14*RCS)和 ILED =。 在连接 J5引脚1和2的情况下、VIADJ 等于1.5V (5V Vref 的分压器)。 因此、将1.5V 代入1A ILED 的 ILED 公式、可以计算出 RCS = 0.107欧姆。 您可以使用0.1欧姆、将 R21更改为28K、得到的确切值为1A。
J5连接的引脚1-2正确
J7连接到引脚2-3、但在 VBAT2不存在的情况下、TPS92692将对输出电流进行内部 PWM 处理。 如果您想在 LED 上运行持续直流电流、则需要有 VBAT2存在或移除 R25
谢谢 Tuan