请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TLV61046A、 LMR62014、 TPS61086你好
我们是否有比 LMR62014/TLV61046A 更高的效率升压解决方案符合以下规格? 谢谢你。
输入电压= 5V
输出电压= 12V
Iout = 510mA
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.