This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LMZ31704:INH 开/关抑制

Guru**** 2589265 points
Other Parts Discussed in Thread: UCD90160, LMZ31704

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/606605/lmz31704-inh-on-off-inhibit

器件型号:LMZ31704
主题中讨论的其他器件:UCD90160

您好!

如果应用需要开/关功能、LMZ37104的数据表建议使用外部开漏/集电极器件(SLVSBV8A 的第19页)。 我有一个控制器(UCD90160)、可生成所需的控制信号。

我的问题是、我是否可以避免使用外部漏极开路器件、而是直接从控制器驱动、并具有外部下拉电阻(大约10kohm)。 如果可能、可以共享 INH 引脚上的内部上拉电流源的详细信息

请注意、在为 LMZ31704提供任何输入电压之前、我的设计中已为控制器加电。