Other Parts Discussed in Thread: LM25118
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM25118您好:
我已准备好设计降压/升压直流/直流转换器电路。
其输入电压为3.6V~4.2V、输出电压为4V。 输出电流为3A。
那么、您会向我推荐一些合适的转换器 IC 吗?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.