Other Parts Discussed in Thread: TPS25750
您好!
在此主题中: TPS25750:禁用灌电流或拉电流(重新访问)-接口论坛-接口- TI E2E 支持论坛 Chuck 提到
The Type C PD standard requires that a 5V PDO be provided if the device is configured as as DRP or a UFP, so there is no way to disable all sourcing unless you define the connection type as a SINK only. I need to think about any method that we could use to force to device into sink only mode. This would resolve the issue that you are seeing.
您是否找到了一种方法来真正关闭灌电流或拉电流?
此致、
Ambroise