This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM5010:60V 至3.3V 应用

Guru**** 2562160 points
Other Parts Discussed in Thread: LM5010

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/597736/lm5010-60v-to-3-3v-application

器件型号:LM5010

电路板电源输入范围为12V 至60V。 当我选择 LM5010时、我想确认能否获得稳定的3.3V@ 1A?

或者、我需要两步转换、例如首先通过 LM5010获取10V、然后使用另一个直流/直流转换器获取3.3V?

您对高压转换为低压应用有什么建议吗?