This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM25085:LM25085:输出随着负载的增加而下降,但高达0.5V

Guru**** 2465780 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/593299/lm25085-lm25085-output-drops-as-the-load-increases-but-as-much-as-0-5v

器件型号:LM25085

我的电路采用7安培电源设计

输入 电压范围为14V 至30V、 应可在8V 至24V 之间进行编程  

我遇到的问题是、当负载超过2安培时、压降将高达0.5V

我监控的 FB 引脚实际上不是1.25V,而是更低? 任何建议得到认可的电路