This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS63050:器件无法正常工作、可以使用帮助

Guru**** 2589245 points
Other Parts Discussed in Thread: TPS63050

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/632542/tps63050-part-not-working-could-use-help

器件型号:TPS63050

TPS63050在新电路板设计上不起作用。

我使用 TPS63050进行了新设计。 该部件似乎在工作、因为引脚1 (L1)正在切换、引脚4的输出电压为0.6V。 分压器(R14/R15)在0.6V 输出下为我提供大约0.125V 的电压。 但引脚5 (FB)在3.8V 输出下绝不会达到0.8V、正如设计所期望的那样。

我已将3.8V 电压直接注入引脚4 (3.8V 总线)、并获得3.8V 电压、同时电路消耗预期的~40mA 电流。

有什么建议吗?