请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS61089 我对 TPS61089有疑问。
数据表列出了4.5V 至12.6V 的输出电压范围、但没有给出4.5V 规格的理由。 FB 电压为1.212V。
我正在考虑使用此 IC 来驱动激光二极管、激光二极管的压降约为4至4.5V。
谢谢你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.