This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS54719:根据数据表公式计算最小输出电压最大值

Guru**** 2510095 points
Other Parts Discussed in Thread: TPS54519, TPS54719

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/568000/tps54719-vout-min-max-calculation-as-per-datasheet-formulae

器件型号:TPS54719
主题中讨论的其他器件:TPS54519

大家好、团队、

我们使用 TPS54719器件以3.3V 作为输入来生成2.5V@5.91A。 随附的是我在4种情况下计算2个器件(TPS54519和 TPS54719)的 Vout 最小值和最大值的电子表格(1.8V@1.36A、1.35V@3.66A、1V@4.84A、2.5V@5.91A、使用3.3V 作为输入+/-5%容差)。 当输出电压为2.5V 时、我将获得最小 Vout 为2.668V、最大 Voutmax 为2.464V。 请查看此内容并建议如何更正设计。  e2e.ti.com/.../3034.G450_5F00_TPS54519_2D00_719-_5F00_Vout_5F00_calc.xlsx