This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS23753A:带负载运行、IC 失败

Guru**** 2589245 points
Other Parts Discussed in Thread: TL431

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/643514/tps23753a-run-with-load-ic-failed

器件型号:TPS23753A
Thread 中讨论的其他器件:TL431

首先、该设计的输出电压为12V、负载可以正常工作。  但是、我们将输出电压更改为18V (将 TL431的电阻调整为5.1k 和33.2k)、开关电源为50V。 我们可以看到它在没有负载的情况下是正常的。

加载、正常启动 (连接90欧姆电阻、电流0.2A、电压18V)、几十秒后、电流为0、芯片烧坏了、原因是什么? 如何解决?