This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] Linux/BQ27441-G1:有关 I2C 通信的一般问题

Guru**** 2589275 points
Other Parts Discussed in Thread: BQ27441-G1

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/659727/linux-bq27441-g1-generic-question-about-i2c-communications

器件型号:BQ27441-G1

工具/软件:Linux

BQ27441-G1手册对我来说有点困惑。  我正在尝试读取电池的剩余电量(0x0c 和0x0d)

我只需要读取这两个值-正确(在本例中为 A904)、那么它的1193mAh 剩余电量是吗?

感谢您的帮助。

$ i2cdump -y 1 0x55
未指定大小(使用字节数据访问)
    0 1 2 3 4 5 6 7 8 9 A b c d e f   0123456789abcdef
00:21 04 76 0b 53 10 A8 00 dc 04 dc 04 A9 04 A8 04   !?v?S???????????????
10:00 00 fd ff 38 ff 3c 05 00 f0 00 64 00 76 0b   ..
20:5A 01 00 53 10 00 AB 04 A9 04 AB 04 A8 04   Z???????????
30:64 00 XX XX XX XX XX XX XX XX XX XX F8 25 3c 05 00   d.XXXXXXXX?%
40:00 00 AB ff 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00..   ?..........
50:00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    
60:00 00 XX XX A5 XX f0 00 c0 03 E6 04 00 00 C5 ff   .XX?X??????..
70:XX XX XX XX XX XX XX XX XX XX XX XX XX XX 66 fe ff 52 10 76 0b   XXXXXXXf?.R?v?
80:21 04 76 0b 53 10 A8 00 dc 04 dc 04 A9 04 A8 04   !?v?S???????????????
90:00 00 fd ff 38 ff 3c 05 00 f0 00 64 00 76 0b   ..
A0:5A 01 00 53 10 00 AB 04 A9 04 AB 04 A8 04   Z?????????????
B0:64 00 XX XX XX XX XX XX XX XX XX F8 25 3c 05 00   d.XXXXXXXX?%
C0:00 AB ff 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00..   ?..........
D0:00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    
E0:00 00 XX XX A5 XX f0 00 c0 03 E6 04 00 C5 ff   .XX?X??????..
F0:XX XX XX XX XX XX XX XX XX XX XX XX XX 66 fe ff 52 10 76 0b   XXXXXXXf?.R?v?