This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LMZ34002:负载或 UVLO 电阻器无输出

Guru**** 2603475 points
Other Parts Discussed in Thread: LMZ34002

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/618238/lmz34002-no-output-with-load-or-with-uvlo-resistors

器件型号:LMZ34002

我使用 LMZ34002通过 Rset 178K 将24VDC 转换为-15VDC。 如果我有2个 UVLO 电阻器(174K 和16K 以将 Von 阈值设置为14V)、则该输出保持为-0.9V。 我没有针对该板的输出开/关控制。 当移除两个电阻器时、如果我断开所有负载、IC 会根据需要输出-15VDC。 如果存在100uF 电容器和轻负载(20K + 1mA LED)、则需要几分钟时间才能导通至-15V。 请提供帮助。