This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS61178:短路行为

Guru**** 2609895 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/640482/tps61178-short-circuit-behavior

器件型号:TPS61178

您好!

查看数据表的图20、当输出发生短路时、器件通过关闭负载断开 FET M1进行响应。  

数据表显示、当负载电流达到20A 或输出电压低于设定点30%时、会检测到短路。

在90毫秒断续关断时间后、我看到器件重新启动、电流一直上升到20A、然后再次关断。 电流是否需要达到该高电平才能再次关断? 由于在接地短路的情况下输出电压将为0V、因此不应比设定的输出电压低30%以上、在达到20A 之前关闭器件?

还是因为器件仍处于启动阶段? 达到20A 限值会中断启动阶段吗?

谢谢!

Ryan B.