请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM25088 尊敬的 TI:
我的客户使用 LM25088、Vin=24V、Vout=12V、空载时输出为12V、 但当负载为1A 时、输出将降至9V、当负载增加时、压降更大。
您能帮助分析 LM25088问题吗? 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.