Other Parts Discussed in Thread: LM25119
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM25119同步整流降压用于电池充电项目、该项目支持连续电流传导模式。
输入:15-20V、输出:13.8V、功率:1.5kW、可安装外部 MOSFET、
以及 TI 是否有适当的器件建议?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.