This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM5175:LM5175EVM 上的降压/升压击穿不稳定性

Guru**** 2766265 points

Other Parts Discussed in Thread: LM5175EVM, LM5175

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/705866/lm5175-buck-boost-on-lm5175evm-shoot-down-with-unstability

器件型号:LM5175

您好!

我将使用输入为12.5V 的 LM5175EVM 板测试 LM5175、为 PC 卡提供有效的应力测试。

我不知道工具生成的负载分布、但我没有检测到过高的电流峰值;有时控制器的12V 输出电压会下降到接近4V、没有明显的电流峰值、但始终与某种不稳定行为同时发生。

在中、以黄色显示了12V 输出、以绿色显示了电流感应 CS 电阻器(R15)上的电压。

有什么想法会导致这种不稳定性和压降电压?

谢谢