请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TPS54824、 TPS54620大家好、团队、
我正在寻找 具有以下特性的降压稳压器:
输入5V 输出4.6V、最大输入电压可超过12V
低高侧和低侧 MOSFET 导通电阻
输出电流可超过4A
低成本更好
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.