请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM2621EVAL 主题中讨论的其他器件:TPS55340、 LM2621、 TPS61230A
我已将电路板连接到 Vin=4.2V、Vout=5V、并且负载的输出电流为0.8A。 但是、考虑到效率图、我测得的效率低于数据表中的效率。 它应该大约为88%、我测量了78%。 近况如何?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.