请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS92692 工具/软件:WEBENCH设计工具
大家好、我们希望获得有关使用 TPS92692的建议和设计帮助。 我们将提供24VDC (10%)、并为高达4安培的电流供电。 我想了解一下、我们是否可以将8个 LED 串联并并联、这样我们就可以获得所需的光长。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.