This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS40200:是否有用于计算该设计最大电流的公式

Guru**** 2589300 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/679392/tps40200-is-there-a-formula-to-calculate-the-max-current-for-the-design

器件型号:TPS40200
Thread 中讨论的其他器件:SwitcherPro

SwitcherPro 指示我在开头输入的3A、但是否有方法来验证/计算它?

感谢您的任何帮助