This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS63710:是否可以使用3个 TPS63710生成3A 输出电流?

Guru**** 2812305 points

Other Parts Discussed in Thread: TPS63710

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/730154/tps63710-can-make-3a-output-current-using-3-tps63710

器件型号:TPS63710

您好!

客户希望在 TPS63710中使用12V 输入电压-3V 输出电流3A 输出电流。

可以使用三个并联的 TPS63710生成3A 输出电流?

如果可以、是否有任何检查点?

此致、

Nicky