Other Parts Discussed in Thread: BQ24075, BQ24075T
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ24075 您好!
根据9.3.6电池组温度监测。
103AT-2型热敏电阻的允许温度范围为0°C 至50°C
我对此有一个问题。
解决方案我将温度范围降低至 0°C 至45°C。通过添加两个外部电阻器?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.