请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS2H160-Q1 尊敬的先生:
TPS2H160-Q1的 CS 功能是否可以测量30mA 和120mA 等低电流? 精度如何? BTW,它可以设置为低于30mA,然后打开通道1,设置为超过120mA,然后打开通道2?Thans。
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的先生:
TPS2H160-Q1的 CS 功能是否可以测量30mA 和120mA 等低电流? 精度如何? BTW,它可以设置为低于30mA,然后打开通道1,设置为超过120mA,然后打开通道2?Thans。
Jason