请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LP8860-Q1 设计
1. LEDs 10S/4P,LED+为33V,但没有指示灯,在 LED- LP8860的输出引脚(21、22、24、25)测试为8V,是什么因素导致了问题?
余量似乎可由 DRV_HEADR[2:0]编程,但其默认值是?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
设计
1. LEDs 10S/4P,LED+为33V,但没有指示灯,在 LED- LP8860的输出引脚(21、22、24、25)测试为8V,是什么因素导致了问题?
余量似乎可由 DRV_HEADR[2:0]编程,但其默认值是?