请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ76930 您好!
我注意 到、在数据表第8.2.1节"设计要求"(第49页)的末尾、最大放电电流设置为10A。
我想知道是否可以将此芯片用于更高功率的应用、例如峰值放电为~100A 的9s10p 电池? 如果不是、TI 是否为此案例提供任何其他解决方案?
谢谢你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.