请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ24133 您好!
1.如果使用12V 输入源为采用 BQ24133的3节(12.6V)锂电池充电、会发生什么情况?
2.是否可以在 BQ24133 AVCC 上使用12V 电压、在 PVCC 上使用15V 电压? 如果是、需要注意哪些事项?
谢谢你。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.