This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LMR23610:CFF 选择

Guru**** 2493545 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/714824/lmr23610-cff-selection

器件型号:LMR23610

你(们)好

COUT = 47uF、CFF = 39pF 通过 WEBENCH 仿真获得、Vin=24V、Vout=3.3V、Iout = 0.3A。

而根据等式(17)和(18)、在以下条件下、CFF 可计算为58pF。

VOUT = 3.3V、

COUT = 47uF (降额后的陶瓷电容器)

RFBT = 51K Ω

如果选择的 CFF 小于计算结果、可以考虑什么影响?

贝斯特雷加兹