Other Parts Discussed in Thread: LM5116
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5116 您好!
当负载电流增加到9A 或10A 时、效率会发生什么情况? 还想知道输入电压增加到50V 或60V 时的效率?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.