This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS40170-EP:支持 MIL-STD 1275和放大器的降压;MIL-STD 461

Guru**** 2387830 points
Other Parts Discussed in Thread: TPS40170-EP
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1235034/tps40170-ep-buck-supporting-mil-std-1275-mil-std-461

器件型号:TPS40170-EP

团队、

您是否可以建议我们使用符合 MIL-STD 1275和 MIL-STD 461标准的降压转换器。

 所需规格如下所示、

输入电压:典型值28V

输出电压:5V 或12V

输出电流:6A 至8A

开关频率范围:200kHz 至800kHz -固定

EMI:辐射发射:-30dBm/MHz (10kHz 至1GHz)

传导发射:-40dBm (10kHz 至1GHz)

纹波:0.5%

功率因数:0.97滞后

噪声:比基频低70dB

隔离:2、000伏 RMS、60Hz

瞬态抗扰度:±500V、µs 50 μ s、持续时间不超过1ms、最大能量为15mJ

工作温度:-55°C 至+85°C

存储温度:-65°C 至+125°C