请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LP5810 由于我们当前的 RGB LED (一个封装中包含3个裸片)、VF > 3.4V。
我们是否可以让 LED 驱动器 IC (TI/LP5810)连接到3.3V 并让白光/RGB 2 LED 连接到5V 电源。
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.