This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPSM63602:这只是降压吗?

Guru**** 2812305 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1322930/tpsm63602-is-this-step-down-only

器件型号:TPSM63602

该部件可通过3V 至36V 的输入输出1V 至16V。 但是、它被称为降压器件。

这是否意味着、对于16V 输出、我必须使用大于16V 的输入电压?

或者、我能否从12V 输入获得16V 输出?

如果是降压(仅限)、T/I 是否具有可以通过12V 输入提供16V 电压的集成式直流/直流模块(2A)?