This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS5430:电感选择

Guru**** 2562180 points
Other Parts Discussed in Thread: TPS5450

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1320421/tps5430-inductance-selection

器件型号:TPS5430
主题中讨论的其他器件:TPS5450

大家好、

我在这里有一个问题、如果我提供30V 输入、15V 输出、但后端负载的电流仅为0.01A

根据计算电感的公式,LMIN=Vout*(Vin-Vout)/(Vin*kid*Iout*fsw )=15*15/(30*0.3*0.01*500000)=0.005

则 LMIN=5000uH。

如果我按照数据表上的典型电路选择22uH 电感、这会是个问题吗?

此外, 如果我交换输出和接地之间的连接,输出是否会变成-15V?在这种情况下,Vout* (Vin-Vout )将保持30*(15-15)或(-15)*(30+15)?