This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS650861:Alder Lake n50

Guru**** 2814505 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1315700/tps650861-alder-lake-n50

器件型号:TPS650861

您好!

是否有适用于  Intel ADL-N (Alder Lake -N) N50 CPU 的 PMIC?

输入电压9 -14V

3 *开关电源

AUX_1.8V_5.5A

1.05V_1.5A

1.8V_2A

 

2个 LDO

3.3V_0.5A

1.24V_ 10mA

谢谢!

杰夫