请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:UCC28951大家好、我想设计一个具有输出电压和电流控制功能的简单 SMPS (输入- 90VAC 至270VAC、输出 V - 60VDC 至80V DC、输出电流- 0至10A)。 谁能为我提供建议或提供参考设计?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
UCC28951。
一个类似的参考设计:
此外、该器件还具有 EVM 600W