请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ24170 您好
BQ24170的 TS 引脚 连接到包括 NTC 10k Ω 电阻器 /热敏电阻在内的电阻器、以防止电池温度过高。
将其连接到电池是否正确? 如果连接到 BQ24170、则它控制的是组件温度而不是电池温度。
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.