请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TPS92640、TPS92641 您好!
我需要用于 LED 驱动器(精确调光)的降压控制器以满足以下规格要求
输入电压:46V 至52V
输入电流:15A
VLED (输出到 LED 条):44V 至50V
ILED (输出):1A 至10A
因此,请尽早建议合适的部分...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.