尊敬的:
对于正在生产的产品、我们需要具有以下规格的直流/直流转换器:
输入40、8到55、2V
输出:5V 1A
50µs 距离:连续:2kV 50Hz、/冲击:5kV (1、2/μ m)
TI 是否有符合这些规格的直流/直流转换器或应用手册来创建一个?
此致
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.