This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS2H000-Q1:TPS2H000BQPWPRQ1

Guru**** 1135430 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1285052/tps2h000-q1-tps2h000bqpwprq1

器件型号:TPS2H000-Q1

器件型号:TPS2H000BQPWPRQ1

在数据表第8页中、"(2)外部电流限制精度仅适用于大于电流限制设置1.5倍的过载情况"。

这意味着  

如果电流限制设置为16mA,电流限制阈值将是16mA * 1.5 = 24mA?

也就是说、如果客户将电流限制设置为16mA、电流限制是否会在24mA 发生故障?

谢谢。