请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ35100EVM-795 主题中讨论的其他器件:BQ35100、 MSP430FR5994、 BQSTUDIO、 EV2400
我将使用 MSP430FR5994通过 I2C 使用命令0x08读取提供给 BQ35100的电压、如下面的代码所示。 我遇到的问题是、如果我使用电源调整供电电压并再次发送命令、我仍将读取初始供应电压。 即使在我重新启动程序时、也没有获得更新的电压。 获得更新电压的唯一方法是下电上电、然后再次运行程序。
我知道在 Battery Management Studio 中、必须首先扫描然后发送 GAUGE_START 命令、以便定期更新寄存器值、但我想知道如何使用我的程序执行此操作。 我曾尝试在此处也使用 GAUGE_START 命令、但我不确定 构建它的适当方式是什么。
TIA!
#include <msp430.h> #include <stdint.h> #include <stdbool.h> //****************************************************************************** // Pin Config ****************************************************************** //****************************************************************************** #define LED_OUT P1OUT #define LED_DIR P1DIR #define LED0_PIN BIT0 #define LED1_PIN BIT1 //****************************************************************************** // Example Commands ************************************************************ //****************************************************************************** #define FUEL_GAUGE_ADDR 0x55 #define MAX_BUFFER_SIZE 20 uint8_t GAUGE_START [1] = {0x0011}; uint8_t Voltage [2] = {0}; //****************************************************************************** // General I2C State Machine *************************************************** //****************************************************************************** typedef enum I2C_ModeEnum{ IDLE_MODE, NACK_MODE, TX_REG_ADDRESS_MODE, RX_REG_ADDRESS_MODE, TX_DATA_MODE, RX_DATA_MODE, SWITCH_TO_RX_MODE, SWITCH_TO_TX_MODE, TIMEOUT_MODE } I2C_Mode; /* Used to track the state of the software state machine*/ I2C_Mode MasterMode = IDLE_MODE; /* The Register Address/Command to use*/ uint8_t TransmitRegAddr = 0; /* ReceiveBuffer: Buffer used to receive data in the ISR * RXByteCtr: Number of bytes left to receive * ReceiveIndex: The index of the next byte to be received in ReceiveBuffer * TransmitBuffer: Buffer used to transmit data in the ISR * TXByteCtr: Number of bytes left to transfer * TransmitIndex: The index of the next byte to be transmitted in TransmitBuffer * */ uint8_t ReceiveBuffer[MAX_BUFFER_SIZE] = {0}; uint8_t RXByteCtr = 0; uint8_t ReceiveIndex = 0; uint8_t TransmitBuffer[MAX_BUFFER_SIZE] = {0}; uint8_t TXByteCtr = 0; uint8_t TransmitIndex = 0; /* For slave device with dev_addr, read the data specified in slaves reg_addr. * The received data is available in ReceiveBuffer * * dev_addr: The slave device address. * Example: SLAVE_ADDR * reg_addr: The register or command to send to the slave. * Example: CMD_TYPE_0_SLAVE * count: The length of data to read * Example: TYPE_0_LENGTH * */ I2C_Mode I2C_Master_ReadReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t count) { /* Initialize state machine */ MasterMode = TX_REG_ADDRESS_MODE; TransmitRegAddr = reg_addr; RXByteCtr = count; TXByteCtr = 0; ReceiveIndex = 0; TransmitIndex = 0; /* Initialize slave address and interrupts */ UCB2I2CSA = dev_addr; UCB2IFG &= ~(UCTXIFG + UCRXIFG); // Clear any pending interrupts UCB2IE &= ~UCRXIE; // Disable RX interrupt UCB2IE |= UCTXIE; // Enable TX interrupt UCB2CTLW0 |= UCTR + UCTXSTT; // I2C TX, start condition __bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupts return MasterMode; } /* For slave device with dev_addr, writes the data specified in *reg_data * * dev_addr: The slave device address. * Example: SLAVE_ADDR * reg_addr: The register or command to send to the slave. * Example: CMD_TYPE_0_MASTER * *reg_data: The buffer to write * Example: MasterType0 * count: The length of *reg_data * Example: TYPE_0_LENGTH * */ I2C_Mode I2C_Master_WriteReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t *reg_data, uint8_t count) { /* Initialize state machine */ MasterMode = TX_REG_ADDRESS_MODE; TransmitRegAddr = reg_addr; //Copy register data to TransmitBuffer CopyArray(reg_data, TransmitBuffer, count); TXByteCtr = count; RXByteCtr = 0; ReceiveIndex = 0; TransmitIndex = 0; /* Initialize slave address and interrupts */ UCB2I2CSA = dev_addr; UCB2IFG &= ~(UCTXIFG + UCRXIFG); // Clear any pending interrupts UCB2IE &= ~UCRXIE; // Disable RX interrupt UCB2IE |= UCTXIE; // Enable TX interrupt UCB2CTLW0 |= UCTR + UCTXSTT; // I2C TX, start condition __bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupts return MasterMode; } void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count) { uint8_t copyIndex = 0; for (copyIndex = 0; copyIndex < count; copyIndex++) { dest[copyIndex] = source[copyIndex]; } } //****************************************************************************** // Device Initialization ******************************************************* //****************************************************************************** void initGPIO() { // Configure GPIO LED_OUT &= ~(LED0_PIN | LED1_PIN); // P1 setup for LED & reset output LED_DIR |= (LED0_PIN | LED1_PIN); // I2C pins P7SEL0 |= BIT0 | BIT1; P7SEL1 &= ~(BIT0 | BIT1); // Disable the GPIO power-on default high-impedance mode to activate // previously configured port settings PM5CTL0 &= ~LOCKLPM5; } void initClockTo16MHz() { // Configure one FRAM waitstate as required by the device datasheet for MCLK // operation beyond 8MHz _before_ configuring the clock system. FRCTL0 = FRCTLPW | NWAITS_1; // Clock System Setup CSCTL0_H = CSKEY_H; // Unlock CS registers CSCTL1 = DCOFSEL_0; // Set DCO to 1MHz // Set SMCLK = MCLK = DCO, ACLK = LFXTCLK (VLOCLK if unavailable) CSCTL2 = SELA__LFXTCLK | SELS__DCOCLK | SELM__DCOCLK; // Per Device Errata set divider to 4 before changing frequency to // prevent out of spec operation from overshoot transient CSCTL3 = DIVA__4 | DIVS__4 | DIVM__4; // Set all corresponding clk sources to divide by 4 for errata CSCTL1 = DCOFSEL_4 | DCORSEL; // Set DCO to 16MHz // Delay by ~10us to let DCO settle. 60 cycles = 20 cycles buffer + (10us / (1/4MHz)) __delay_cycles(60); CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers to 1 for 16MHz operation CSCTL0_H = 0; // Lock CS registers } void initI2C() { UCB2CTLW0 = UCSWRST; // Enable SW reset UCB2CTLW0 |= UCMODE_3 | UCMST | UCSSEL__SMCLK | UCSYNC; // I2C master mode, SMCLK UCB2BRW = 160; // fSCL = SMCLK/160 = ~100kHz UCB2I2CSA = FUEL_GAUGE_ADDR; // Slave Address UCB2CTLW0 &= ~UCSWRST; // Clear SW reset, resume operation UCB2IE |= UCNACKIE; } //****************************************************************************** // Main ************************************************************************ //****************************************************************************** int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer initClockTo16MHz(); initGPIO(); initI2C(); I2C_Master_ReadReg(FUEL_GAUGE_ADDR, 0x08, 2); // Read voltage register CopyArray(ReceiveBuffer, Voltage, 2); I2C_Master_WriteReg(FUEL_GAUGE_ADDR, 0x3e, GAUGE_START, 1); I2C_Master_ReadReg(FUEL_GAUGE_ADDR, 0x08, 2); // Read voltage register CopyArray(ReceiveBuffer, Voltage, 2); __bis_SR_register(LPM0_bits + GIE); return 0; } //****************************************************************************** // I2C Interrupt *************************************************************** //****************************************************************************** #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = USCI_B2_VECTOR __interrupt void USCI_B2_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(USCI_B2_VECTOR))) USCI_B2_ISR (void) #else #error Compiler not supported! #endif { //Must read from UCB2RXBUF uint8_t rx_val = 0; switch(__even_in_range(UCB2IV, USCI_I2C_UCBIT9IFG)) { case USCI_NONE: break; // Vector 0: No interrupts case USCI_I2C_UCALIFG: break; // Vector 2: ALIFG case USCI_I2C_UCNACKIFG: // Vector 4: NACKIFG break; case USCI_I2C_UCSTTIFG: break; // Vector 6: STTIFG case USCI_I2C_UCSTPIFG: break; // Vector 8: STPIFG case USCI_I2C_UCRXIFG3: break; // Vector 10: RXIFG3 case USCI_I2C_UCTXIFG3: break; // Vector 12: TXIFG3 case USCI_I2C_UCRXIFG2: break; // Vector 14: RXIFG2 case USCI_I2C_UCTXIFG2: break; // Vector 16: TXIFG2 case USCI_I2C_UCRXIFG1: break; // Vector 18: RXIFG1 case USCI_I2C_UCTXIFG1: break; // Vector 20: TXIFG1 case USCI_I2C_UCRXIFG0: // Vector 22: RXIFG0 rx_val = UCB2RXBUF; if (RXByteCtr) { ReceiveBuffer[ReceiveIndex++] = rx_val; RXByteCtr--; } if (RXByteCtr == 1) { UCB2CTLW0 |= UCTXSTP; } else if (RXByteCtr == 0) { UCB2IE &= ~UCRXIE; MasterMode = IDLE_MODE; __bic_SR_register_on_exit(CPUOFF); // Exit LPM0 } break; case USCI_I2C_UCTXIFG0: // Vector 24: TXIFG0 switch (MasterMode) { case TX_REG_ADDRESS_MODE: UCB2TXBUF = TransmitRegAddr; if (RXByteCtr) MasterMode = SWITCH_TO_RX_MODE; // Need to start receiving now else MasterMode = TX_DATA_MODE; // Continue to transmission with the data in Transmit Buffer break; case SWITCH_TO_RX_MODE: UCB2IE |= UCRXIE; // Enable RX interrupt UCB2IE &= ~UCTXIE; // Disable TX interrupt UCB2CTLW0 &= ~UCTR; // Switch to receiver MasterMode = RX_DATA_MODE; // State state is to receive data UCB2CTLW0 |= UCTXSTT; // Send repeated start if (RXByteCtr == 1) { //Must send stop since this is the N-1 byte while((UCB2CTLW0 & UCTXSTT)); UCB2CTLW0 |= UCTXSTP; // Send stop condition } break; case TX_DATA_MODE: if (TXByteCtr) { UCB2TXBUF = TransmitBuffer[TransmitIndex++]; TXByteCtr--; } else { //Done with transmission UCB2CTLW0 |= UCTXSTP; // Send stop condition MasterMode = IDLE_MODE; UCB2IE &= ~UCTXIE; // disable TX interrupt __bic_SR_register_on_exit(CPUOFF); // Exit LPM0 } break; default: __no_operation(); break; } break; default: break; } }