请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TPS40210团队、
若要从3.3V 输入生成隔离式14V 输出电压/ 100mA、我们最具成本效益的方式是哪种拓扑和器件型号?
谢谢。
-凯文
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.