请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ28Z610-R1 我对2S1P 电池使用 BQ28Z610-R1、放电到25% 电压时为6738mV、10秒后跳到0%、 电压为6698mV、为什么会发生这种情况?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我对2S1P 电池使用 BQ28Z610-R1、放电到25% 电压时为6738mV、10秒后跳到0%、 电压为6698mV、为什么会发生这种情况?