Other Parts Discussed in Thread: TLV62130
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TLV62130 团队成员
我们在 产品中使用 TLV62130RGTR,我们要求使用2 9V 电池(9V MN1604 /尺寸:9V (6LP3146 ) )串联,它将变成18伏。 自建议的最大电压为17V 以来、使用18V 是否安全??
谢谢、此致
阿什瓦特
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.