请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ40Z50 主题中讨论的其他器件: BQ4050
对于 BQ4050和 BQ40z50、我的理解是、当放电大于寄存器中设置的周期计数阈值时、将对周期计数。 如果我的阈值设置为80%、并且放电和充电25% 4次、此值会计为1个周期吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.