This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 电池组和充电器建议

Guru**** 2390735 points
Other Parts Discussed in Thread: BQ40Z50, BQ7718, BQ2962
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1263338/battery-pack-and-charger-recommendation

主题中讨论的其他器件:BQ40Z50BQ7718BQ2962

迪亚尔斯、

对于2款具有主要参数的新产品(电池组和充电器)、请推荐3款 IC (电量监测计 IC、保护 IC 和充电器 IC):

     电池组:(电量监测计 IC、保护 IC)

        电池:4S1P

        充电:16.8V+/- 0.2V、0至50 ℃ 时4A,0.5mA 低于0℃

        放电:最大10A、持续6.5A

        通信接口:SMBus

        

        充电器:(充电器 IC)

        充电电压:16.8V+/- 0.2V

        最大电池充电电流:0.5mA < 0C (最大值)、0C < 4A < 50C

        通信接口:SMBus