This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ISO5451-Q1:VCC1最大消耗电流

Guru**** 2560390 points
Other Parts Discussed in Thread: ISO5451-Q1

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1260288/iso5451-q1-vcc1-maximum-consumption-current

器件型号:ISO5451-Q1

大家好、

您可以帮助检查 VCC1=5V 是否最大消耗电流为245mA 吗? 非常感谢您的支持来确认。

此致

Jie