This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ76952:未稳定 STM32F103 I2C 与 BQ76952之间的通信。

Guru**** 2589265 points
Other Parts Discussed in Thread: BQ34Z100-G1, BQ76952, BQSTUDIO

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1241182/bq76952-stm32f103-i2c-communication-with-bq76952-is-not-stablished

器件型号:BQ76952
主题中讨论的其他器件: BQSTUDIO、BQ34Z100-G1

您好先生,长期以来我一直在尝试与 BQ76952和 STM32F103 viz. I2C 通信时,我还连接示波器观看 SDL 和 SCL 的图像 ,我也附加了图像,在设置相同的后,我总是变得不需要(在我的理解)  像这样的数据(例如单元读数、温度)。

7880mV
7880mV
7880mV
7880mV
10450mV
10450mV
10450mV
10450mV
10450mV
10450mV
7880mV
7880mV
7880mV
7880mV
 

,  

/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * <h2><center>Copyright Copyright (c) 2023 STMicroelectronics.
  * All rights reserved.</center></h2>
  *
  * This software component is licensed by ST under BSD 3-Clause license,
  * the "License"; You may not use this file except in compliance with the
  * License. You may obtain a copy of the License at:
  *                        opensource.org/licenses/BSD-3-Clause
  *
  ******************************************************************************
  */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include <stdio.h>
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
#define DEV_ADDR  0x10  // BQ769x2 address is 0x10 including R/W bit or 0x8 as 7-bit address
#define CRC_Mode 0  // 0 for disabled, 1 for enabled
#define MAX_BUFFER_SIZE     10
/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1;

TIM_HandleTypeDef htim1;

UART_HandleTypeDef huart1;

/* USER CODE BEGIN PV */
uint8_t spiData [2];
uint8_t spiRxData [2];
uint8_t rxdata [2];
uint8_t busyData [2] = {0xFF, 0xFF};

uint8_t TX_2Byte [2] = {0x00, 0x00};
uint8_t TX_3Byte [3] = {0x00, 0x00, 0x00};
uint8_t TX_4Byte [4] = {0x00, 0x00, 0x00, 0x00};
uint8_t TX_Buffer [MAX_BUFFER_SIZE] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};

uint8_t RX_2Byte [2] = {0x00, 0x00};
uint8_t RX_3Byte [3] = {0x00, 0x00, 0x00};
uint8_t RX_4Byte [4] = {0x00, 0x00, 0x00, 0x00};
uint8_t RX_12Byte [12] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
uint8_t RX_Buffer [MAX_BUFFER_SIZE] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
unsigned int RX_CRC_Check = 0;

// Variables for cell voltages, temperatures, CC2 current, Stack voltage, PACK Pin voltage, LD Pin voltage
uint16_t CellVoltage [16] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
float Temperature [3] = {0,0,0};
float FET_Temperature = 0;
uint16_t Stack_Voltage = 0x00;
uint16_t LD_Voltage = 0x00;
uint16_t PACK_Voltage = 0x00;
uint16_t PACK_Current = 0x00;
uint16_t AlarmBits = 0x00;

uint8_t SafetyStatusA;  // Safety Status Register A
uint8_t SafetyStatusB;  // Safety Status Register B
uint8_t SafetyStatusC;  // Safety Status Register C
uint8_t PFStatusA;   // Permanent Fail Status Register A
uint8_t PFStatusB;   // Permanent Fail Status Register B
uint8_t PFStatusC;   // Permanent Fail Status Register C
uint8_t FET_Status;  // FET Status register contents See TRM Section 12.2.20  - Shows states of FETs

uint16_t CB_ActiveCells;  // Cell Balancing Active Cells
uint16_t DEVICE_NUMBER;

uint8_t	UV_Fault = 0;   // under-voltage fault state
uint8_t	OV_Fault = 0;   // over-voltage fault state
uint8_t	SCD_Fault = 0;  // short-circuit fault state
uint8_t	OCD_Fault = 0;  // over-current fault state
uint8_t LD_ON = 0;							// Load Detect status bit
uint8_t DCHG = 0;   // discharge FET state
uint8_t CHG = 0;   // charge FET state
uint8_t PCHG = 0;  // pre-charge FET state
uint8_t PDSG = 0;  // pre-discharge FET state

uint32_t AccumulatedCharge_Int;
uint32_t AccumulatedCharge_Frac;
uint32_t AccumulatedCharge_Time;
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
static void MX_TIM1_Init(void);
static void MX_USART1_UART_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void uprint(char * str)
{
	HAL_UART_Transmit(&huart1, (uint8_t*)str, strlen(str), 100);
}
/* USER CODE END 0 */
void delayUS(uint32_t us) {   // Sets the delay in microseconds.
	__HAL_TIM_SET_COUNTER(&htim1,0);  // set the counter value a 0
	while (__HAL_TIM_GET_COUNTER(&htim1) < us);  // wait for the counter to reach the us input in the parameter
}

void delay_ticks(uint32_t ticks)
{
    SysTick->LOAD = ticks;
    SysTick->VAL = 0;
    SysTick->CTRL = SysTick_CTRL_ENABLE_Msk;
    // COUNTFLAG is a bit that is set to 1 when counter reaches 0.
    // It's automatically cleared when read.
    while ((SysTick->CTRL & SysTick_CTRL_COUNTFLAG_Msk) == 0);
    SysTick->CTRL = 0;
}

void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
{
    uint8_t copyIndex = 0;
    for (copyIndex = 0; copyIndex < count; copyIndex++)
    {
        dest[copyIndex] = source[copyIndex];
    }
}

unsigned char Checksum(unsigned char *ptr, unsigned char len)
	// Calculates the checksum when writing to a RAM register. The checksum is the inverse of the sum of the bytes.
{
	unsigned char i;
	unsigned char checksum = 0;

	for(i=0; i<len; i++)
		checksum += ptr[i];

	checksum = 0xff & ~checksum;

	return(checksum);
}



unsigned char CRC8(unsigned char *ptr, unsigned char len)
{
	unsigned char i;
	unsigned char crc=0;
	while(len--!=0)
	{
		for(i=0x80; i!=0; i/=2)
		{
			if((crc & 0x80) != 0)
			{
				crc *= 2;
				crc ^= 0x107;
			}
			else
				crc *= 2;

			if((*ptr & i)!=0)
				crc ^= 0x107;
		}
		ptr++;
	}
	return(crc);
}

void I2C_WriteReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
{
		#if CRC_Mode
		{
		uint8_t crc_count = 0;
		crc_count = count * 2;
		uint8_t crc1stByteBuffer [3] = {0x10, reg_addr, reg_data[0]};
		unsigned int j;
		unsigned int i;
		uint8_t temp_crc_buffer [3];

		TX_Buffer[0] = reg_data[0];
		TX_Buffer[1] = CRC8(crc1stByteBuffer,3);

		j = 2;
		for(i=1; i<count; i++)
		{
			TX_Buffer[j] = reg_data[i];
			j = j + 1;
			temp_crc_buffer[0] = reg_data[i];
			TX_Buffer[j] = CRC8(temp_crc_buffer,1);
			j = j + 1;
		}
		HAL_I2C_Mem_Write(&hi2c1, DEV_ADDR, reg_addr, 1, TX_Buffer, count, 1000);
		}
		#endif

		#if CRC_Mode < 1
			HAL_I2C_Mem_Write(&hi2c1, DEV_ADDR, reg_addr, 1, reg_data, count, 1000);
		#endif
}


int I2C_ReadReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
{
	unsigned int RX_CRC_Fail = 0;  // reset to 0. If in CRC Mode and CRC fails, this will be incremented.

	#if CRC_Mode
	{
		uint8_t crc_count = 0;
		uint8_t ReceiveBuffer [10] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
		crc_count = count * 2;
		unsigned int j;
		unsigned int i;
		unsigned char CRCc = 0;
		uint8_t temp_crc_buffer [3];

		HAL_I2C_Mem_Read(&hi2c1, DEV_ADDR, reg_addr, 1, ReceiveBuffer, crc_count, 1000);
		uint8_t crc1stByteBuffer [4] = {0x10, reg_addr, 0x11, ReceiveBuffer[0]};
		CRCc = CRC8(crc1stByteBuffer,4);
		if (CRCc != ReceiveBuffer[1])
			RX_CRC_Fail += 1;

		RX_Buffer[0] = ReceiveBuffer[0];

		j = 2;
		for (i=1; i<count; i++)
		{
			RX_Buffer[i] = ReceiveBuffer[j];
			temp_crc_buffer[0] = ReceiveBuffer[j];
			j = j + 1;
			CRCc = CRC8(temp_crc_buffer,1);
			if (CRCc != ReceiveBuffer[j])
				RX_CRC_Fail += 1;
			j = j + 1;
		}
		CopyArray(RX_Buffer, reg_data, crc_count);
	}
	#endif

	#if CRC_Mode < 1
			HAL_I2C_Mem_Read(&hi2c1, DEV_ADDR, reg_addr, 1, reg_data, count, 1000);
	#endif

	  return 0;
}


void AFE_Reset() {
	// Reset command. Resets all registers to default values or the values programmed in OTP.
	TX_2Byte[0] = 0x12; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_Init() {
	// Configures all parameters in device RAM

	// Enter CONFIGUPDATE mode (Subcommand 0x0090) - It is required to be in CONFIG_UPDATE mode to program the device RAM settings
	// See TRM Section 7.6 for full description of CONFIG_UPDATE mode
	TX_2Byte[0] = 0x90; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);

	delayUS(2000);

	// After entering CONFIG_UPDATE mode, RAM registers can be programmed. When programming RAM, checksum and length must also be
	// programmed for the change to take effect. All of the RAM registers are described in detail in Chapter 13 of the BQ76952 TRM.
	// An easier way to find the descriptions is in the BQStudio Data Memory screen. When you move the mouse over the register name,
	// a full description of the register and the bits will pop up on the screen.
	// A summary of the Data Memory is also in Section 13.9 of the TRM.

	// 'Power Config' - Set DSLP_LDO  - 0x9234 = 0x2D82  (See TRM section 13.3.2)
	// Setting the DSLP_LDO bit allows the LDOs to remain active when the device goes into Deep Sleep mode
  TX_4Byte[0] = 0x34; TX_4Byte[1] = 0x92; TX_4Byte[2] = 0x82; TX_4Byte[3] = 0x2D;
  I2C_WriteReg(0x3E, TX_4Byte, 4);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06;  // Checksum and Length
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// 'REG0 Config' - set REG0_EN bit to enable pre-regulator
	TX_3Byte[0] = 0x37; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x01;
  I2C_WriteReg(0x3E, TX_3Byte, 3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// 'REG12 Config' - Enable REG1 with 3.3V output
	TX_3Byte[0] = 0x36; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x0D;
  I2C_WriteReg(0x3E, TX_3Byte, 3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// 'VCell Mode' - Enable 16 cells - 0x9304 = 0x0000  (See TRM section 13.3.2.19)
	// 0x0000 sets the default value of 16 cells.
  TX_4Byte[0] = 0x04; TX_4Byte[1] = 0x93; TX_4Byte[2] = 0x00; TX_4Byte[3] = 0x00;
  I2C_WriteReg(0x3E, TX_4Byte, 4);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06;  // Checksum and Length
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// 'Default Alarm Mask' - Enable FullScan and ADScan bits
	// 0xF882
  TX_4Byte[0] = 0x6D; TX_4Byte[1] = 0x92; TX_4Byte[2] = 0x82; TX_4Byte[3] = 0xF8;
  I2C_WriteReg(0x3E, TX_4Byte, 4);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06;  // Checksum and Length
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// Enable protections in 'Enabled Protections A' 0x9261 = 0xBC (See TRM section 13.3.3.2)
	// Enables SCD (short-circuit), OCD1 (over-current in discharge), OCC (over-current in charge),
	// COV (over-voltage), CUV (under-voltage)
	TX_3Byte[0] = 0x61; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0xFC;
  I2C_WriteReg(0x3E, TX_3Byte, 3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// Enable all protections in 'Enabled Protections B' 0x9262 = 0xF7 (See TRM section 13.3.3.3)
	// Enables OTF (over-temperature FET), OTINT (internal over-temperature), OTD (over-temperature in discharge),
	// OTC (over-temperature in charge), UTINT (internal under-temperature), UTD (under-temperature in discharge), UTC (under-temperature in charge)
	TX_3Byte[0] = 0x62; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0xF7;
  I2C_WriteReg(0x3E, TX_3Byte, 3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// Set TS1 to measure Cell Temperature - 0x92FD = 0x07   (See TRM Section 13.3.2.12)
	TX_3Byte[0] = 0xFD; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x07;
  I2C_WriteReg(0x3E, TX_3Byte, 3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// Set TS3 to measure FET Temperature - 0x92FF = 0x0F   (See TRM Section 13.3.2.14)
	TX_3Byte[0] = 0xFF; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x0F;
  I2C_WriteReg(0x3E, TX_3Byte, 3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// Set DFETOFF pin to control BOTH CHG and DSG FET - 0x92FB = 0x42 (set to 0x00 to disable)
	// See TRM section 13.3.2.10, Table 13-7
	TX_3Byte[0] = 0xFB; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x42;
  I2C_WriteReg(0x3E, TX_3Byte, 3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// Set up Alert Pin - 0x92FC = 0x2A  - See TRM Section 13.3.2.11, Table 13-8
	// This configures the Alert pin to drive high (REG1 voltage) when enabled.
	// Other options available include active-low, drive HiZ, drive using REG18 (1.8V), weak internal pull-up and pull-down
	TX_3Byte[0] = 0xFC; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x2A;
  I2C_WriteReg(0x3E, TX_3Byte, 3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);


	// Set up Cell Balancing Configuration - 0x9335 = 0x03   -  Automated balancing while in Relax or Charge modes
	// See TRM Section 13.3.11. Chapter 10 of TRM describes Cell Balancing in detail
	// Also see "Cell Balancing with BQ76952, BQ76942 Battery Monitors" document on ti.com
	TX_3Byte[0] = 0x35; TX_3Byte[1] = 0x93; TX_3Byte[2] = 0x03;
  I2C_WriteReg(0x3E, TX_3Byte, 3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// Set up COV (over-voltage) Threshold - 0x9278 = 0x55 (4301 mV)
	// COV Threshold is this value multiplied by 50.6mV  See TRM section 13.6.2
	TX_3Byte[0] = 0x78; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x55;
  I2C_WriteReg(0x3E, TX_3Byte, 3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// Set up SCD Threshold - 0x9286 = 0x05 (100 mV = 100A across 1mOhm sense resistor)
	// See TRM section 13.6.7    0x05=100mV
	TX_3Byte[0] = 0x86; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x05;
  I2C_WriteReg(0x3E, TX_3Byte, 3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// Set up SCD Delay - 0x9287 = 0x03 (30 us)    See TRM section 13.6.7
	// Units of 15us
	TX_3Byte[0] = 0x87; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x03;
  I2C_WriteReg(0x3E, TX_3Byte, 3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);

	// Set up SCDL Latch Limit to 1 to set SCD recovery only with load removal 0x9295 = 0x01
	// If this is not set, then SCD will recover based on time (SCD Recovery Time parameter).
	// See TRM section 13.6.11.1
	TX_3Byte[0] = 0x95; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x01;
  I2C_WriteReg(0x3E, TX_3Byte, 3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
	delayUS(1000);


	// Exit CONFIGUPDATE mode  - Subcommand 0x0092
	TX_2Byte[0] = 0x92; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
	delayUS(1000);
}

//  ********************************* FET Control Commands  ***************************************

void AFE_FET_ENABLE() {
	// Toggles the FET_EN bit in the Manufacturing Status register. So this command can be used to enable or disable the FETs.
	TX_2Byte[0] = 0x22; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_FET_Control(uint8_t FET_states) {  // Bit3 = PCHG_OFF, Bit 2 = CHG_OFF, Bit1 = PDSG_OFF, Bit 0 = DSG_OFF
	TX_3Byte[0] = 0x97; TX_3Byte[1] = 0x00; TX_3Byte[2] = FET_states;
	I2C_WriteReg(0x3E,TX_3Byte,3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  I2C_WriteReg(0x60, TX_2Byte, 2);
}

void DSG_PDSG_OFF() {
	// Disable discharge (and pre-discharge) FETs
	// Subcommand 0x0093  See TRM Table 5-8  (DSG_PDSG_OFF())
	TX_2Byte[0] = 0x93; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
}

void CHG_PCHG_OFF() {
	// Disable charge (and pre-charge) FETs
	// Subcommand 0x0094  See TRM Table 5-8  (CHG_PCHG_OFF())
	TX_2Byte[0] = 0x94; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_ALL_FETS_OFF() {
	// Disable all FETs with command 0x0095  See TRM Table 5-8
	TX_2Byte[0] = 0x95; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_ALL_FETS_ON() {
	// All all FETs to be enabled with command 0x0096  See TRM Table 5-8
	TX_2Byte[0] = 0x96; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_BOTHOFF () {
	// Disables all FETs using the DFETOFF (BOTHOFF) pin
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_SET);  // DFETOFF pin (BOTHOFF) set low
}

void AFE_RESET_BOTHOFF () {
	// Resets DFETOFF (BOTHOFF) pin
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);  // DFETOFF pin (BOTHOFF) set low
}

void AFE_ReadFETStatus() {
	// Read FET Status to see which FETs are enabled
	I2C_ReadReg(0x7F, RX_2Byte, 2);
  FET_Status = (RX_2Byte[1]*256 + RX_2Byte[0]);
	DCHG = 0x4 & RX_2Byte[0];   // discharge FET state
	CHG = 0x1 & RX_2Byte[0];   // charge FET state
	PCHG = 0x2 & RX_2Byte[0];  // pre-charge FET state
	PDSG = 0x8 & RX_2Byte[0];  // pre-discharge FET state
}



// ********************************* End of FET Control Commands *********************************


// ********************************* AFE Cell Balancing Commands   *****************************************

void CB_ACTIVE_CELLS() {
	// Check status of which cells are balancing
	TX_2Byte[0] = 0x83; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
	I2C_ReadReg(0x40, RX_2Byte, 2);
  CB_ActiveCells = (RX_2Byte[1]*256 + RX_2Byte[0]);
}


// ********************************* End of AFE Cell Balancing Commands   *****************************************


// ********************************* AFE Power Commands   *****************************************
void AFE_DeepSleep() {
	// Puts the device into DEEPSLEEP mode. See TRM section 7.4
	TX_2Byte[0] = 0x0F; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
	I2C_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_ExitDeepSleep() {
	// Exits DEEPSLEEP mode. See TRM section 7.4
	TX_2Byte[0] = 0x0E; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_ShutdownCommand() {
	// Puts the device into SHUTDOWN mode. See TRM section 7.5
	TX_2Byte[0] = 0x10; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_ShutdownPin() {
	// Puts the device into SHUTDOWN mode using the RST_SHUT pin
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_SET);  // Sets RST_SHUT pin
}

void AFE_ReleaseShutdownPin() {
	// Releases the RST_SHUT pin
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);  // Resets RST_SHUT pin
}

void AFE_SLEEP_ENABLE() { // SLEEP_ENABLE 0x0099
	// Allows the device to enter Sleep mode if current is below Sleep Current. See TRM section 7.3
	TX_2Byte[0] = 0x99; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_SLEEP_DISABLE() { // SLEEP_DISABLE 0x009A
	// Takes the device out of sleep mode. See TRM section 7.3
	TX_2Byte[0] = 0x9A; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
}

// ********************************* End of AFE Power Commands   *****************************************


// ********************************* AFE Status and Fault Commands   *****************************************

uint16_t AFE_ReadAlarmStatus() {
	// Read this register to find out why the Alert pin was asserted. See section 6.6 of the TRM for full description.
	I2C_ReadReg(0x62, RX_2Byte, 2);
	return (RX_2Byte[1]*256 + RX_2Byte[0]);
}

void AFE_ReadSafetyStatus() {
	// Read Safety Status A/B/C and find which bits are set
	// This shows which primary protections have been triggered
	I2C_ReadReg(0x03, RX_2Byte, 2);
	SafetyStatusA = (RX_2Byte[1]*256 + RX_2Byte[0]);
	UV_Fault = 0x4 & RX_2Byte[0];
	OV_Fault = 0x8 & RX_2Byte[0];
	SCD_Fault = 0x8 & RX_2Byte[1];
	OCD_Fault = 0x2 & RX_2Byte[1];
	I2C_ReadReg(0x05, RX_2Byte, 2);
	SafetyStatusB = (RX_2Byte[1]*256 + RX_2Byte[0]);
	I2C_ReadReg(0x07, RX_2Byte, 2);
	SafetyStatusC = (RX_2Byte[1]*256 + RX_2Byte[0]);
}

void AFE_ReadPFStatus() {
	// Read Permanent Fail Status A/B/C and find which bits are set
	// This shows which permanent failures have been triggered
	I2C_ReadReg(0x0B, RX_2Byte, 2);
	PFStatusA = (RX_2Byte[1]*256 + RX_2Byte[0]);
	I2C_ReadReg(0x0D, RX_2Byte, 2);
	PFStatusB = (RX_2Byte[1]*256 + RX_2Byte[0]);
	I2C_ReadReg(0x0F, RX_2Byte, 2);
	PFStatusC = (RX_2Byte[1]*256 + RX_2Byte[0]);
}


void AFE_ControlStatus() {
	// Control status register - Bit0 - LD_ON (load detected)
	// See TRM Table 6-1
	I2C_ReadReg(0x00, RX_2Byte, 2);
  LD_ON = 0x1 & RX_2Byte[0];
}

void AFE_BatteryStatus() {
	// Battery status register - See TRM Table 6-2
	I2C_ReadReg(0x12, RX_2Byte, 2);
}

void AFE_ClearFaults() {
	TX_2Byte[0] = 0x00; TX_2Byte[1] = 0xF8;
	I2C_WriteReg(0x62,TX_2Byte,2);
}

void AFE_ClearScanBits() {
	TX_2Byte[0] = 0x82; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x62,TX_2Byte,2);
}

void AFE_PFReset() {
	TX_2Byte[0] = 0x29; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
}

uint16_t AFE_DeviceID() {
	// Read Device ID using Subcommand 0x0001
	TX_2Byte[0] = 0x01; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
	delayUS(500);
	I2C_ReadReg(0x40, RX_2Byte, 2);
	return (RX_2Byte[1]*256 + RX_2Byte[0]);
}
// ********************************* End of AFE Status and Fault Commands   *****************************************


// ********************************* AFE Measurement Commands   *****************************************

uint16_t AFE_ReadCellVoltage(uint8_t channel) {
	I2C_ReadReg(channel*2+0x12, RX_2Byte, 2);
	return (RX_2Byte[1]*256 + RX_2Byte[0]);     // cell voltage is reported in mV
}

uint16_t AFE_ReadStackVoltage() {
	I2C_ReadReg(0x34, RX_2Byte, 2);
	return 10 * (RX_2Byte[1]*256 + RX_2Byte[0]);  // voltage is reported in 0.01V units
}

uint16_t AFE_ReadPackVoltage() {
	I2C_ReadReg(0x36, RX_2Byte, 2);
	return 10 * (RX_2Byte[1]*256 + RX_2Byte[0]);  // voltage is reported in 0.01V units
}

uint16_t AFE_ReadLDVoltage() {
	I2C_ReadReg(0x38, RX_2Byte, 2);
	return 10 * (RX_2Byte[1]*256 + RX_2Byte[0]);  // voltage is reported in 0.01V units
}

uint16_t AFE_ReadCurrent() {
	I2C_ReadReg(0x3A, RX_2Byte, 2);
	return (RX_2Byte[1]*256 + RX_2Byte[0]);  // current is reported in mA
}



float AFE_ReadTemperature(uint8_t channel) {
	switch(channel)
	{
		case 0:
			I2C_ReadReg(0x70, RX_2Byte, 2);  // TS1 pin
			break;
		case 1:
			I2C_ReadReg(0x74, RX_2Byte, 2);  // TS3 pin, FET temperature
			break;
		default: break;
	}
	return (0.1 * (float)(RX_2Byte[1]*256 + RX_2Byte[0])) - 273.15;  // convert from 0.1K to Celcius
}


void AFE_ReadPassQ() {
	// Read Accumulated Charge and Time from DASTATUS6 (See TRM Table 4-6)
	TX_2Byte[0] = 0x76; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
	delayUS(1000);
	I2C_ReadReg(0x40, RX_12Byte, 12);
	AccumulatedCharge_Int = ((RX_12Byte[3]<<24) + (RX_12Byte[2]<<16) + (RX_12Byte[1]<<8) + RX_12Byte[0]);
	AccumulatedCharge_Frac = ((RX_12Byte[7]<<24) + (RX_12Byte[6]<<16) + (RX_12Byte[5]<<8) + RX_12Byte[4]);
	AccumulatedCharge_Time = ((RX_12Byte[11]<<24) + (RX_12Byte[10]<<16) + (RX_12Byte[9]<<8) + RX_12Byte[8]);
}

void AFE_ClearPassQ() {
	// Clear Accumulated Charge and Time, command 0x0082
	TX_2Byte[0] = 0x82; TX_2Byte[1] = 0x00;
	I2C_WriteReg(0x3E,TX_2Byte,2);
}

// *********************************
/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */
	uint8_t	I2C_Return;
  /* USER CODE END 1 */
	volatile int i = 0;
	char uart_buf[50];
	int uart_buf_len;
  /* USER CODE END 1 */
	uint16_t CellVoltage1 =0;
  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_I2C1_Init();
  MX_TIM1_Init();
  MX_USART1_UART_Init();
  /* USER CODE BEGIN 2 */
  HAL_TIM_Base_Start(&htim1);

  	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);  // RST_SHUT pin set low
  	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);  // DFETOFF pin (BOTHOFF) set low
      delayUS(10000);


  	AFE_Reset();
  	delayUS(60000);
  	AFE_Init();
  	delayUS(10000);
  	AFE_FET_ENABLE();
  	delayUS(10000);

  	AFE_SLEEP_DISABLE();

  	delayUS(60000); delayUS(60000); delayUS(60000); delayUS(60000);  //wait to start measurements after FETs close
  	CellVoltage[1] = AFE_ReadCellVoltage(1);
  	CellVoltage[5] = AFE_ReadCellVoltage(5);
  	CellVoltage[10] = AFE_ReadCellVoltage(10);
  	Stack_Voltage = AFE_ReadStackVoltage();
  	PACK_Voltage = AFE_ReadPackVoltage();
  	LD_Voltage = AFE_ReadLDVoltage();
  	PACK_Current = AFE_ReadCurrent();
  	Temperature[0] = AFE_ReadTemperature(0)m   ;
  	FET_Temperature = AFE_ReadTemperature(1);
  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
	  CellVoltage1 =0;
    /* USER CODE END WHILE */
	  CellVoltage1 = AFE_ReadCellVoltage(1);
	  Stack_Voltage = AFE_ReadStackVoltage();
	//Debug code - prints the Cell1 Voltage to a terminal window
	uart_buf_len = sprintf(uart_buf, "%u mV\r\n", Temperature[1] );
	HAL_UART_Transmit(&huart1, (uint8_t *)uart_buf, uart_buf_len, 100);
	CellVoltage1 =0;
	CellVoltage[2] = AFE_ReadCellVoltage(2);

	CellVoltage[3] = AFE_ReadCellVoltage(3);
	CellVoltage[4] = AFE_ReadCellVoltage(4);
	CellVoltage[5] = AFE_ReadCellVoltage(5);
	CellVoltage[6] = AFE_ReadCellVoltage(6);
	CellVoltage[7] = AFE_ReadCellVoltage(7);
	CellVoltage[8] = AFE_ReadCellVoltage(8);
	CellVoltage[9] = AFE_ReadCellVoltage(9);
	CellVoltage[10] = AFE_ReadCellVoltage(10);
	//Stack_Voltage = AFE_ReadStackVoltage();
	PACK_Voltage = AFE_ReadPackVoltage();
	LD_Voltage = AFE_ReadLDVoltage();
	PACK_Current = AFE_ReadCurrent();
	Temperature[0] = AFE_ReadTemperature(2);
	FET_Temperature = AFE_ReadTemperature(1);

	AlarmBits = AFE_ReadAlarmStatus();
	//Debug code - prints the Cell1 Voltage to a terminal window
	// 		uart_buf_len = sprintf(uart_buf, "%u \r\n", AlarmBits);
	//	HAL_UART_Transmit(&huart1, (uint8_t *)uart_buf, uart_buf_len, 100);

	if (AlarmBits & 0x82) {
		AFE_ClearScanBits();
	}

	if (AlarmBits & 0xC000) {
		AFE_ReadSafetyStatus();
		AFE_ReadPFStatus();
		AFE_ClearFaults();
		AFE_PFReset();
	}
	CellVoltage1 =0;
	HAL_Delay(500);
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON;
  RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL8;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
  {
    Error_Handler();
  }
}

/**
  * @brief I2C1 Initialization Function
  * @param None
  * @retval None
  */
static void MX_I2C1_Init(void)
{


	  /* USER CODE BEGIN I2C1_Init 0 */

	  /* USER CODE END I2C1_Init 0 */

	  /* USER CODE BEGIN I2C1_Init 1 */

	  /* USER CODE END I2C1_Init 1 */
	  hi2c1.Instance = I2C1;
	  hi2c1.Init.ClockSpeed = 400000;
	  hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
	  hi2c1.Init.OwnAddress1 = 0;
	  hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
	  hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
	  hi2c1.Init.OwnAddress2 = 0;
	  hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
	  hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
	  if (HAL_I2C_Init(&hi2c1) != HAL_OK)
	  {
	    Error_Handler();
	  }
	  /* USER CODE BEGIN I2C1_Init 2 */

	  /* USER CODE END I2C1_Init 2 */

}

/**
  * @brief TIM1 Initialization Function
  * @param None
  * @retval None
  */
static void MX_TIM1_Init(void)
{

  /* USER CODE BEGIN TIM1_Init 0 */

  /* USER CODE END TIM1_Init 0 */

  TIM_ClockConfigTypeDef sClockSourceConfig = {0};
  TIM_MasterConfigTypeDef sMasterConfig = {0};

  /* USER CODE BEGIN TIM1_Init 1 */

  /* USER CODE END TIM1_Init 1 */
  htim1.Instance = TIM1;
  htim1.Init.Prescaler = 63;
  htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
  htim1.Init.Period = 65535;
  htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
  htim1.Init.RepetitionCounter = 0;
  htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
  if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
  {
    Error_Handler();
  }
  sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
  if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
  {
    Error_Handler();
  }
  sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
  if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN TIM1_Init 2 */

  /* USER CODE END TIM1_Init 2 */

}

/**
  * @brief USART1 Initialization Function
  * @param None
  * @retval None
  */
static void MX_USART1_UART_Init(void)
{

  /* USER CODE BEGIN USART1_Init 0 */

  /* USER CODE END USART1_Init 0 */

  /* USER CODE BEGIN USART1_Init 1 */

  /* USER CODE END USART1_Init 1 */
  huart1.Instance = USART1;
  huart1.Init.BaudRate = 115200;
  huart1.Init.WordLength = UART_WORDLENGTH_8B;
  huart1.Init.StopBits = UART_STOPBITS_1;
  huart1.Init.Parity = UART_PARITY_NONE;
  huart1.Init.Mode = UART_MODE_TX_RX;
  huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart1.Init.OverSampling = UART_OVERSAMPLING_16;
  if (HAL_UART_Init(&huart1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN USART1_Init 2 */

  /* USER CODE END USART1_Init 2 */

}

/**
  * @brief GPIO Initialization Function
  * @param None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOD_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13, GPIO_PIN_RESET);

  /*Configure GPIO pin : PC13 */
  GPIO_InitStruct.Pin = GPIO_PIN_13;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */
void HAL_GPIO_EXTI_Callback ( uint16_t GPIO_Pin )
{
	if ( GPIO_Pin == GPIO_PIN_3 ) {
		HAL_GPIO_TogglePin (GPIOA, GPIO_PIN_5 );
	}
	else {
		__NOP ();
	}
}
/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @param  file: pointer to the source file name
  * @param  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

我很高兴你重播...

谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Arjun:

    我有几个简短的问题:

    1.能否将 PCB 的完整原理图发送出去?

    2.对于信号的照片,您是否可以使用数字逻辑分析仪来查看信号,以便我们可以查看发送的内容以及是否接收到 ACK 位。

    3.您的设备是否使用 CRC 检查进行传输? 默认情况下、BQ7695202启用了 CRC、如果 MCU 不期望 CRC 出现、它会更改您发送和接收的信号。

    此致!

    A·内德尔费尔德

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的评分

    1.好的,先生,我会附上的。

    2、没有 SIR 除了 示波器我没有逻辑分析仪。

    3.我不知道 BQ7695202默认启用了 CRC 、在程序中我禁用了相同的功能。 这可能是原因,我会尝试相同 的,并恢复您相同的角度。

    #先生,现在我能够读取所有数据,但我不能写入任何东西 BQ7xxx

    这是我在 main 函数中做的例子 ,并试图在写入后读取 COV 阈值电压,但它只显示我的默认数据, COV 寄存器没有变化

    ////////////////////////////////////////////////////////////////////////// COV -THS-73////////////////////////////////////////////////////////

    //进入 configupdate 模式-子命令0x0090
    TX_2Byte[0]= 0x90;
    TX_2Byte[1]= 0x00;
    I2C_WriteReg (0x3E、TX_2字节、2);
    第36集7.3分庭(2000年);

    //0x9278是地址, 0x55是数据

    TX_3Byte[0]= 0x78;
    TX_3Byte[1]= 0x92;
    TX_3Byte[2]= 0x50;    
    I2C_WriteReg (0x3E、TX_3Byte、3);
    DELAYUS(1000);

    //表示校验和及长度

    TX_2Byte[0]=校验和(TX_3Byte,3);
    TX_2Byte[1]= 0x05;
    I2C_WriteReg (0x60、TX_2字节、2);
    READ_COV_TH =(RX_2Byte[1]*256 + RX_2Byte[0]);
    DELAYUS(1000);


    //退出 configupdate 模式-子命令0x0092
    TX_2Byte[0]= 0x92;TX_2Byte[1]= 0x00;
    I2C_WriteReg (0x3E、TX_2字节、2);
    DELAYUS(1000);

    ////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    ////////////////////////////////////////////////////////////////////////// COV -THS-73////////////////////////////////////////////////////////
    TX_2Byte[0]= 0x90;
    TX_2Byte[1]= 0x00;
    I2C_WriteReg (0x3E、TX_2字节、2);
    第36集7.3分庭(2000年);

    // 1. 将地址的低位字节写入0x3E (本例中为0x78)。
    // 2. 将地址的高位字节写入0x3F (本例中为0x92)。
    // 3. 将数据存储器值以小端字节序的格式写入传输缓冲区(0x40至0x5F)。 注:最多32个
    //字节的数据存储器可以写入一次块写入。 在本例中、将0x7A 写入0x40、将0x30写入
    // 0x41。
    // 4. 将写入数据的校验和(本例中为0x44)写入0x60、并将数据长度(本例中为0x06)写入
    //示例)转换到0x61中。

    TX_3Byte[0]= 0x78;
    TX_3Byte[1]= 0x92;
    TX_3Byte[2]= 0x10;
    I2C_WriteReg (0x3E、TX_3Byte、3);
    DELAYUS(1000);
    TX_2Byte[0]=校验和(TX_3Byte,3);
    TX_2Byte[1]= 0x05;
    I2C_WriteReg (0x60、TX_2字节、2);
    DELAYUS(1000);

    // 5. 可以通过读回数据来对其进行验证。 将地址的低位字节写入0x3E (0x80)、将高位字节
    //地址字节到0x3F (0x91)。
    // 6. 从0x61读取响应的长度。 传输缓冲区将填充一个32字节的数据块、因此
    //长度将是36个字节,或在本例中为0x24。
    // 7. 从0x40开始读取数据长度的缓冲区。 Calibration:Voltage:Cell 1 Gain 的新值为
    //在0x40 (0x7A)和0x41 (0x30)中看到。
    // 8. 读取0x60处的校验和并验证其是否与为整个传输缓冲区读取的数据匹配

    TX_2Byte[0]= 0x00;
    TX_2Byte[1]= 0x00;
    I2C_ReadReg (0x40、TX_2字节、2);
    CB_ActiveCells =(RX_2Byte[1]*256 + RX_2Byte[0]);
    DELAYUS(1000);


    //退出 configupdate 模式-子命令0x0092
    TX_2Byte[0]= 0x92;TX_2Byte[1]= 0x00;
    I2C_WriteReg (0x3E、TX_2字节、2);
    DELAYUS(1000);

    ////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    #1 使用作为变量的 CB_ActiveCells

    # 2 IIN 评论部分的代码我做了一些更改我的 reff...

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Arjun:

    您是否可以通过检查0x12 Battery Status ()[CFGUPDATE]标志来确认您的设备是否进入 CONFIG_UPDATE 模式? 要进入 CONFIG_UPDATE 模式、器件需要处于 FULLACCESS 模式。 您的器件可能处于 SEALED 或 UNSEALED 模式、这种模式允许读取但不允许写入。 可以通过查看0x12 Battery Status ()[SEC1、SEC0]并查看它们是否为[0、1]来验证这一点、这意味着器件处于 FULLACCESS 状态。 有关此设置的更多信息、您可以查看 TRM 中的第8.1节

    此致!

    A·内德尔费尔德

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、先生!

    我检查了  已设置为[0,1](  8位和9位)的位 Status()[SEC1, SEC0], 我仍然无法对 写 操作进行 ASSCESS。  

    还有一点我想提的是,正如这里显示的两个代码在 TI 网站上提供相同的(旧的和新的一个)通过新的一个,我不能读任何东西,通过旧的一个, 这个问题也是如此、但有一个优点是、我只能  通过更改后使用相同的函数来 RAED "叠加电压" ONELY (因为它运行良好、所以我使用相同的函数读取其他数据(EG)。 温度,电池1-CELL16)   

    我真的不知道发生了什么,我要求请,如果你 给我简单的代码读写操作,然后请指导我的步骤;

    谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

       

    此输出结果,当 I DEBUGE 与新(附在下面)代码. 这样、即使我也无法读取 TS1、  

    我重新检查每个问题、但没有结果 I OTTED、

    #include "main.h"
    #include <stdio.h>
    #include "BQ769x2Header.h"
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    #define DEV_ADDR  0x10  // BQ769x2 address is 0x10 including R/W bit or 0x8 as 7-bit address
    #define CRC_Mode 1  // 0 for disabled, 1 for enabled
    #define MAX_BUFFER_SIZE 10
    #define R 0 // Read; Used in DirectCommands and Subcommands functions
    #define W 1 // Write; Used in DirectCommands and Subcommands functions
    #define W2 2 // Write data with two bytes; Used in Subcommands function
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    I2C_HandleTypeDef hi2c1;
    
    TIM_HandleTypeDef htim1;
    
    UART_HandleTypeDef huart1;
    
    /* USER CODE BEGIN PV */
    uint8_t RX_data [2] = {0x00, 0x00}; // used in several functions to store data read from BQ769x2
    uint8_t RX_32Byte [32] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
    	0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
    	//used in Subcommands read function
    // Global Variables for cell voltages, temperatures, Stack voltage, PACK Pin voltage, LD Pin voltage, CC2 current
    uint16_t CellVoltage [16] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    float Temperature [3] = {0,0,0};
    uint16_t Stack_Voltage = 0x00;
    uint16_t Pack_Voltage = 0x00;
    uint16_t LD_Voltage = 0x00;
    uint16_t Pack_Current = 0x00;
    
    uint16_t AlarmBits = 0x00;
    uint8_t value_SafetyStatusA;  // Safety Status Register A
    uint8_t value_SafetyStatusB;  // Safety Status Register B
    uint8_t value_SafetyStatusC;  // Safety Status Register C
    uint8_t value_PFStatusA;   // Permanent Fail Status Register A
    uint8_t value_PFStatusB;   // Permanent Fail Status Register B
    uint8_t value_PFStatusC;   // Permanent Fail Status Register C
    uint8_t FET_Status;  // FET Status register contents  - Shows states of FETs
    uint16_t CB_ActiveCells;  // Cell Balancing Active Cells
    
    uint8_t	UV_Fault = 0;   // under-voltage fault state
    uint8_t	OV_Fault = 0;   // over-voltage fault state
    uint8_t	SCD_Fault = 0;  // short-circuit fault state
    uint8_t	OCD_Fault = 0;  // over-current fault state
    uint8_t ProtectionsTriggered = 0; // Set to 1 if any protection triggers
    
    uint8_t LD_ON = 0;	// Load Detect status bit
    uint8_t DSG = 0;   // discharge FET state
    uint8_t CHG = 0;   // charge FET state
    uint8_t PCHG = 0;  // pre-charge FET state
    uint8_t PDSG = 0;  // pre-discharge FET state
    
    uint32_t AccumulatedCharge_Int; // in BQ769x2_READPASSQ func
    uint32_t AccumulatedCharge_Frac;// in BQ769x2_READPASSQ func
    uint32_t AccumulatedCharge_Time;// in BQ769x2_READPASSQ func
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_I2C1_Init(void);
    static void MX_TIM1_Init(void);
    static void MX_USART1_UART_Init(void);
    /* USER CODE BEGIN PFP */
    
    /* USER CODE END PFP */
    
    
    void delayUS(uint32_t us) {   // Sets the delay in microseconds.
    	__HAL_TIM_SET_COUNTER(&htim1,0);  // set the counter value a 0
    	while (__HAL_TIM_GET_COUNTER(&htim1) < us);  // wait for the counter to reach the us input in the parameter
    }
    
    void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
    {
        uint8_t copyIndex = 0;
        for (copyIndex = 0; copyIndex < count; copyIndex++)
        {
            dest[copyIndex] = source[copyIndex];
        }
    }
    
    unsigned char Checksum(unsigned char *ptr, unsigned char len)
    // Calculates the checksum when writing to a RAM register. The checksum is the inverse of the sum of the bytes.
    {
    	unsigned char i;
    	unsigned char checksum = 0;
    
    	for(i=0; i<len; i++)
    		checksum += ptr[i];
    
    	checksum = 0xff & ~checksum;
    
    	return(checksum);
    }
    
    unsigned char CRC8(unsigned char *ptr, unsigned char len)
    //Calculates CRC8 for passed bytes. Used in i2c read and write functions
    {
    	unsigned char i;
    	unsigned char crc=0;
    	while(len--!=0)
    	{
    		for(i=0x80; i!=0; i/=2)
    		{
    			if((crc & 0x80) != 0)
    			{
    				crc *= 2;
    				crc ^= 0x107;
    			}
    			else
    				crc *= 2;
    
    			if((*ptr & i)!=0)
    				crc ^= 0x107;
    		}
    		ptr++;
    	}
    	return(crc);
    }
    
    void I2C_WriteReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
    {
    	uint8_t TX_Buffer [MAX_BUFFER_SIZE] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    #if CRC_Mode
    	{
    		uint8_t crc_count = 0;
    		crc_count = count * 2;
    		uint8_t crc1stByteBuffer [3] = {0x10, reg_addr, reg_data[0]};
    		unsigned int j;
    		unsigned int i;
    		uint8_t temp_crc_buffer [3];
    
    		TX_Buffer[0] = reg_data[0];
    		TX_Buffer[1] = CRC8(crc1stByteBuffer,3);
    
    		j = 2;
    		for(i=1; i<count; i++)
    		{
    			TX_Buffer[j] = reg_data[i];
    			j = j + 1;
    			temp_crc_buffer[0] = reg_data[i];
    			TX_Buffer[j] = CRC8(temp_crc_buffer,1);
    			j = j + 1;
    		}
    		HAL_I2C_Mem_Write(&hi2c1, DEV_ADDR, reg_addr, 1, TX_Buffer, crc_count, 1000);
    	}
    #else
    	HAL_I2C_Mem_Write(&hi2c1, DEV_ADDR, reg_addr, 1, reg_data, count, 1000);
    #endif
    }
    
    int I2C_ReadReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
    {
    	unsigned int RX_CRC_Fail = 0;  // reset to 0. If in CRC Mode and CRC fails, this will be incremented.
    	uint8_t RX_Buffer [MAX_BUFFER_SIZE] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    #if CRC_Mode
    	{
    		uint8_t crc_count = 0;
    		uint8_t ReceiveBuffer [10] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    		crc_count = count * 2;
    		unsigned int j;
    		unsigned int i;
    		unsigned char CRCc = 0;
    		uint8_t temp_crc_buffer [3];
    
    		HAL_I2C_Mem_Read(&hi2c1, DEV_ADDR, reg_addr, 1, ReceiveBuffer, crc_count, 1000);
    		uint8_t crc1stByteBuffer [4] = {0x10, reg_addr, 0x11, ReceiveBuffer[0]};
    		CRCc = CRC8(crc1stByteBuffer,4);
    		if (CRCc != ReceiveBuffer[1])
    		{
    			RX_CRC_Fail += 1;
    		}
    		RX_Buffer[0] = ReceiveBuffer[0];
    
    		j = 2;
    		for (i=1; i<count; i++)
    		{
    			RX_Buffer[i] = ReceiveBuffer[j];
    			temp_crc_buffer[0] = ReceiveBuffer[j];
    			j = j + 1;
    			CRCc = CRC8(temp_crc_buffer,1);
    			if (CRCc != ReceiveBuffer[j])
    				RX_CRC_Fail += 1;
    			j = j + 1;
    		}
    		CopyArray(RX_Buffer, reg_data, crc_count);
    	}
    #else
    	HAL_I2C_Mem_Read(&hi2c1, DEV_ADDR, reg_addr, 1, reg_data, count, 1000);
    #endif
    	return 0;
    }
    
    void BQ769x2_SetRegister(uint16_t reg_addr, uint32_t reg_data, uint8_t datalen)
    {
    	uint8_t TX_Buffer[2] = {0x00, 0x00};
    	uint8_t TX_RegData[6] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
    
    	//TX_RegData in little endian format
    	TX_RegData[0] = reg_addr & 0xff;
    	TX_RegData[1] = (reg_addr >> 8) & 0xff;
    	TX_RegData[2] = reg_data & 0xff; //1st byte of data
    
    	switch(datalen)
        {
    		case 1: //1 byte datalength
          		I2C_WriteReg(0x3E, TX_RegData, 3);
    			delayUS(2000);
    			TX_Buffer[0] = Checksum(TX_RegData, 3);
    			TX_Buffer[1] = 0x05; //combined length of register address and data
          		I2C_WriteReg(0x60, TX_Buffer, 2); // Write the checksum and length
    			delayUS(2000);
    			break;
    		case 2: //2 byte datalength
    			TX_RegData[3] = (reg_data >> 8) & 0xff;
    			I2C_WriteReg(0x3E, TX_RegData, 4);
    			delayUS(2000);
    			TX_Buffer[0] = Checksum(TX_RegData, 4);
    			TX_Buffer[1] = 0x06; //combined length of register address and data
          		I2C_WriteReg(0x60, TX_Buffer, 2); // Write the checksum and length
    			delayUS(2000);
    			break;
    		case 4: //4 byte datalength, Only used for CCGain and Capacity Gain
    			TX_RegData[3] = (reg_data >> 8) & 0xff;
    			TX_RegData[4] = (reg_data >> 16) & 0xff;
    			TX_RegData[5] = (reg_data >> 24) & 0xff;
    			I2C_WriteReg(0x3E, TX_RegData, 6);
    			delayUS(2000);
    			TX_Buffer[0] = Checksum(TX_RegData, 6);
    			TX_Buffer[1] = 0x08; //combined length of register address and data
          		I2C_WriteReg(0x60, TX_Buffer, 2); // Write the checksum and length
    			delayUS(2000);
    			break;
        }
    }
    
    void CommandSubcommands(uint16_t command) //For Command only Subcommands
    // See the TRM or the BQ76952 header file for a full list of Command-only subcommands
    {	//For DEEPSLEEP/SHUTDOWN subcommand you will need to call this function twice consecutively
    
    	uint8_t TX_Reg[2] = {0x00, 0x00};
    
    	//TX_Reg in little endian format
    	TX_Reg[0] = command & 0xff;
    	TX_Reg[1] = (command >> 8) & 0xff;
    
    	I2C_WriteReg(0x3E,TX_Reg,2);
    	delayUS(2000);
    }
    
    void Subcommands(uint16_t command, uint16_t data, uint8_t type)
    // See the TRM or the BQ76952 header file for a full list of Subcommands
    {
    	//security keys and Manu_data writes dont work with this function (reading these commands works)
    	//max readback size is 32 bytes i.e. DASTATUS, CUV/COV snapshot
    	uint8_t TX_Reg[4] = {0x00, 0x00, 0x00, 0x00};
    	uint8_t TX_Buffer[2] = {0x00, 0x00};
    
    	//TX_Reg in little endian format
    	TX_Reg[0] = command & 0xff;
    	TX_Reg[1] = (command >> 8) & 0xff;
    
    	if (type == R) {//read
    		I2C_WriteReg(0x3E,TX_Reg,2);
    		delayUS(2000);
    		I2C_ReadReg(0x40, RX_32Byte, 32); //RX_32Byte is a global variable
    	}
    	else if (type == W) {
    		//FET_Control, REG12_Control
    		TX_Reg[2] = data & 0xff;
    		I2C_WriteReg(0x3E,TX_Reg,3);
    		delayUS(1000);
    		TX_Buffer[0] = Checksum(TX_Reg, 3);
    		TX_Buffer[1] = 0x05; //combined length of registers address and data
    		I2C_WriteReg(0x60, TX_Buffer, 2);
    		delayUS(1000);
    	}
    	else if (type == W2){ //write data with 2 bytes
    		//CB_Active_Cells, CB_SET_LVL
    		TX_Reg[2] = data & 0xff;
    		TX_Reg[3] = (data >> 8) & 0xff;
    		I2C_WriteReg(0x3E,TX_Reg,4);
    		delayUS(1000);
    		TX_Buffer[0] = Checksum(TX_Reg, 4);
    		TX_Buffer[1] = 0x06; //combined length of registers address and data
    		I2C_WriteReg(0x60, TX_Buffer, 2);
    		delayUS(1000);
    	}
    }
    
    void DirectCommands(uint8_t command, uint16_t data, uint8_t type)
    // See the TRM or the BQ76952 header file for a full list of Direct Commands
    {	//type: R = read, W = write
    	uint8_t TX_data[2] = {0x00, 0x00};
    
    	//little endian format
    	TX_data[0] = data & 0xff;
    	TX_data[1] = (data >> 8) & 0xff;
    
    	if (type == R) {//Read
    		I2C_ReadReg(command, RX_data, 2); //RX_data is a global variable
    		delayUS(2000);
    	}
    	if (type == W) {//write
        //Control_status, alarm_status, alarm_enable all 2 bytes long
    		I2C_WriteReg(command,TX_data,2);
    		delayUS(2000);
    	}
    }
    
    void BQ769x2_Init() {
    	// Configures all parameters in device RAM
    
    	// Enter CONFIGUPDATE mode (Subcommand 0x0090) - It is required to be in CONFIG_UPDATE mode to program the device RAM settings
    	// See TRM for full description of CONFIG_UPDATE mode
    	CommandSubcommands(SET_CFGUPDATE);
    
    	// After entering CONFIG_UPDATE mode, RAM registers can be programmed. When programming RAM, checksum and length must also be
    	// programmed for the change to take effect. All of the RAM registers are described in detail in the BQ769x2 TRM.
    	// An easier way to find the descriptions is in the BQStudio Data Memory screen. When you move the mouse over the register name,
    	// a full description of the register and the bits will pop up on the screen.
    
    	// 'Power Config' - 0x9234 = 0x2D80
    	// Setting the DSLP_LDO bit allows the LDOs to remain active when the device goes into Deep Sleep mode
      	// Set wake speed bits to 00 for best performance
    	BQ769x2_SetRegister(PowerConfig, 0x2D80, 2);
    
    	// 'REG0 Config' - set REG0_EN bit to enable pre-regulator
    	BQ769x2_SetRegister(REG0Config, 0x01, 1);
    
    	// 'REG12 Config' - Enable REG1 with 3.3V output (0x0D for 3.3V, 0x0F for 5V)
    	BQ769x2_SetRegister(REG12Config, 0x0D, 1);
    
    	// Set DFETOFF pin to control BOTH CHG and DSG FET - 0x92FB = 0x42 (set to 0x00 to disable)
    	BQ769x2_SetRegister(DFETOFFPinConfig, 0x42, 1);
    
    	// Set up ALERT Pin - 0x92FC = 0x2A
    	// This configures the ALERT pin to drive high (REG1 voltage) when enabled.
    	// The ALERT pin can be used as an interrupt to the MCU when a protection has triggered or new measurements are available
    	BQ769x2_SetRegister(ALERTPinConfig, 0x2A, 1);
    
    	// Set TS1 to measure Cell Temperature - 0x92FD = 0x07
    	BQ769x2_SetRegister(TS1Config, 0x07, 1);
    
    	// Set TS3 to measure FET Temperature - 0x92FF = 0x0F
    	BQ769x2_SetRegister(TS3Config, 0x0F, 1);
    
    	// Set HDQ to measure Cell Temperature - 0x9300 = 0x07
    	BQ769x2_SetRegister(HDQPinConfig, 0x00, 1);  // No thermistor installed on EVM HDQ pin, so set to 0x00
    
    	// 'VCell Mode' - Enable 16 cells - 0x9304 = 0x0000; Writing 0x0000 sets the default of 16 cells
    	BQ769x2_SetRegister(VCellMode, 0x0000, 2);
    
    	// Enable protections in 'Enabled Protections A' 0x9261 = 0xBC
    	// Enables SCD (short-circuit), OCD1 (over-current in discharge), OCC (over-current in charge),
    	// COV (over-voltage), CUV (under-voltage)
    	BQ769x2_SetRegister(EnabledProtectionsA, 0xBC, 1);
    
    	// Enable all protections in 'Enabled Protections B' 0x9262 = 0xF7
    	// Enables OTF (over-temperature FET), OTINT (internal over-temperature), OTD (over-temperature in discharge),
    	// OTC (over-temperature in charge), UTINT (internal under-temperature), UTD (under-temperature in discharge), UTC (under-temperature in charge)
    	BQ769x2_SetRegister(EnabledProtectionsB, 0xF7, 1);
    
    	// 'Default Alarm Mask' - 0x..82 Enables the FullScan and ADScan bits, default value = 0xF800
    	BQ769x2_SetRegister(DefaultAlarmMask, 0xF882, 2);
    
    	// Set up Cell Balancing Configuration - 0x9335 = 0x03   -  Automated balancing while in Relax or Charge modes
    	// Also see "Cell Balancing with BQ769x2 Battery Monitors" document on ti.com
    	BQ769x2_SetRegister(BalancingConfiguration, 0x03, 1);
    
    	// Set up CUV (under-voltage) Threshold - 0x9275 = 0x31 (2479 mV)
    	// CUV Threshold is this value multiplied by 50.6mV
    	BQ769x2_SetRegister(CUVThreshold, 0x31, 1);
    
    	// Set up COV (over-voltage) Threshold - 0x9278 = 0x55 (4301 mV)
    	// COV Threshold is this value multiplied by 50.6mV
    	BQ769x2_SetRegister(COVThreshold, 0x55, 1);
    
    	// Set up OCC (over-current in charge) Threshold - 0x9280 = 0x05 (10 mV = 10A across 1mOhm sense resistor) Units in 2mV
    	BQ769x2_SetRegister(OCCThreshold, 0x05, 1);
    
    	// Set up OCD1 Threshold - 0x9282 = 0x0A (20 mV = 20A across 1mOhm sense resistor) units of 2mV
    	BQ769x2_SetRegister(OCD1Threshold, 0x0A, 1);
    
    	// Set up SCD Threshold - 0x9286 = 0x05 (100 mV = 100A across 1mOhm sense resistor)  0x05=100mV
    	BQ769x2_SetRegister(SCDThreshold, 0x05, 1);
    
    	// Set up SCD Delay - 0x9287 = 0x03 (30 us) Enabled with a delay of (value - 1) * 15 µs; min value of 1
    	BQ769x2_SetRegister(SCDDelay, 0x03, 1);
    
    	// Set up SCDL Latch Limit to 1 to set SCD recovery only with load removal 0x9295 = 0x01
    	// If this is not set, then SCD will recover based on time (SCD Recovery Time parameter).
    	BQ769x2_SetRegister(SCDLLatchLimit, 0x01, 1);
    
    	// Exit CONFIGUPDATE mode  - Subcommand 0x0092
    	CommandSubcommands(EXIT_CFGUPDATE);
    }
    
    //  ********************************* FET Control Commands  ***************************************
    
    void BQ769x2_BOTHOFF () {
    	// Disables all FETs using the DFETOFF (BOTHOFF) pin
    	// The DFETOFF pin on the BQ76952EVM should be connected to the MCU board to use this function
    //	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_SET);  // DFETOFF pin (BOTHOFF) set high
    }
    
    void BQ769x2_RESET_BOTHOFF () {
    	// Resets DFETOFF (BOTHOFF) pin
    	// The DFETOFF pin on the BQ76952EVM should be connected to the MCU board to use this function
    	//HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);  // DFETOFF pin (BOTHOFF) set low
    }
    
    void BQ769x2_ReadFETStatus() {
    	// Read FET Status to see which FETs are enabled
    	DirectCommands(FETStatus, 0x00, R);
    	FET_Status = (RX_data[1]*256 + RX_data[0]);
    	DSG = ((0x4 & RX_data[0])>>2);// discharge FET state
      	CHG = (0x1 & RX_data[0]);// charge FET state
      	PCHG = ((0x2 & RX_data[0])>>1);// pre-charge FET state
      	PDSG = ((0x8 & RX_data[0])>>3);// pre-discharge FET state
    }
    
    // ********************************* End of FET Control Commands *********************************
    
    // ********************************* BQ769x2 Power Commands   *****************************************
    
    void BQ769x2_ShutdownPin() {
    	// Puts the device into SHUTDOWN mode using the RST_SHUT pin
    	// The RST_SHUT pin on the BQ76952EVM should be connected to the MCU board to use this function
    	//HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_SET);  // Sets RST_SHUT pin
    }
    
    void BQ769x2_ReleaseShutdownPin() {
    	// Releases the RST_SHUT pin
    	// The RST_SHUT pin on the BQ76952EVM should be connected to the MCU board to use this function
    	//HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);  // Resets RST_SHUT pin
    }
    
    // ********************************* End of BQ769x2 Power Commands   *****************************************
    
    
    // ********************************* BQ769x2 Status and Fault Commands   *****************************************
    
    
    
    void BQ769x2_ReadSafetyStatus() { //good example functions
    	// Read Safety Status A/B/C and find which bits are set
    	// This shows which primary protections have been triggered
    	DirectCommands(SafetyStatusA, 0x00, R);
    	value_SafetyStatusA = (RX_data[1]*256 + RX_data[0]);
    	//Example Fault Flags
    	UV_Fault = ((0x4 & RX_data[0])>>2);
    	OV_Fault = ((0x8 & RX_data[0])>>3);
    	SCD_Fault = ((0x8 & RX_data[1])>>3);
    	OCD_Fault = ((0x2 & RX_data[1])>>1);
    	DirectCommands(SafetyStatusB, 0x00, R);
    	value_SafetyStatusB = (RX_data[1]*256 + RX_data[0]);
    	DirectCommands(SafetyStatusC, 0x00, R);
    	value_SafetyStatusC = (RX_data[1]*256 + RX_data[0]);
    	if ((value_SafetyStatusA + value_SafetyStatusB + value_SafetyStatusC) > 1) {
    		ProtectionsTriggered = 1; }
    	else {
    		ProtectionsTriggered = 0; }
    }
    
    void BQ769x2_ReadPFStatus() {
    	// Read Permanent Fail Status A/B/C and find which bits are set
    	// This shows which permanent failures have been triggered
    	DirectCommands(PFStatusA, 0x00, R);
    	value_PFStatusA = (RX_data[1]*256 + RX_data[0]);
    	DirectCommands(PFStatusB, 0x00, R);
    	value_PFStatusB = (RX_data[1]*256 + RX_data[0]);
    	DirectCommands(PFStatusC, 0x00, R);
    	value_PFStatusC = (RX_data[1]*256 + RX_data[0]);
    }
    
    // ********************************* End of BQ769x2 Status and Fault Commands   *****************************************
    
    
    // ********************************* BQ769x2 Measurement Commands   *****************************************
    
    
    uint16_t BQ769x2_ReadVoltage(uint8_t command)
    // This function can be used to read a specific cell voltage or stack / pack / LD voltage
    {
    	//RX_data is global var
    	DirectCommands(command, 0x00, R);
    	if(command >= Cell1Voltage && command <= Cell16Voltage) {//Cells 1 through 16 (0x14 to 0x32)
    		return (RX_data[1]*256 + RX_data[0]); //voltage is reported in mV
    	}
    	else {//stack, Pack, LD
    		return 10 * (RX_data[1]*256 + RX_data[0]); //voltage is reported in 0.01V units
    	}
    
    }
    void BQ769x2_ReadAllVoltages()
    // Reads all cell voltages, Stack voltage, PACK pin voltage, and LD pin voltage
    {
      int cellvoltageholder = Cell1Voltage; //Cell1Voltage is 0x14
      for (int x = 0; x < 16; x++){//Reads all cell voltages
        CellVoltage[x] = BQ769x2_ReadVoltage(cellvoltageholder);
        cellvoltageholder = cellvoltageholder + 2;
      }
      Stack_Voltage = BQ769x2_ReadVoltage(StackVoltage);
      Pack_Voltage = BQ769x2_ReadVoltage(0x36);
      LD_Voltage = BQ769x2_ReadVoltage(LDPinVoltage);
    }
    
    uint16_t BQ769x2_ReadCurrent()
    // Reads PACK current
    {
    	DirectCommands(CC2Current, 0x00, R);
    	return (RX_data[1]*256 + RX_data[0]);  // current is reported in mA
    }
    
    float BQ769x2_ReadTemperature(uint8_t command)
    {
    	DirectCommands(command, 0x00, R);
    	//RX_data is a global var
    	return (0.1 * (float)(RX_data[1]*256 + RX_data[0])) - 273.15;  // converts from 0.1K to Celcius
    }
    
    void BQ769x2_ReadPassQ(){ // Read Accumulated Charge and Time from DASTATUS6
    	Subcommands(DASTATUS6, 0x00, R);
    	AccumulatedCharge_Int = ((RX_32Byte[3]<<24) + (RX_32Byte[2]<<16) + (RX_32Byte[1]<<8) + RX_32Byte[0]); //Bytes 0-3
    	AccumulatedCharge_Frac = ((RX_32Byte[7]<<24) + (RX_32Byte[6]<<16) + (RX_32Byte[5]<<8) + RX_32Byte[4]); //Bytes 4-7
    	AccumulatedCharge_Time = ((RX_32Byte[11]<<24) + (RX_32Byte[10]<<16) + (RX_32Byte[9]<<8) + RX_32Byte[8]); //Bytes 8-11
    }
    
    // ********************************* End of BQ769x2 Measurement Commands   *****************************************
    
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    
    /* USER CODE END 0 */
    
    /**
      * @brief  The application entry point.
      * @retval int
      */
    int main(void)
    {
      /* USER CODE BEGIN 1 */
        	volatile int i = 0;
    		char uart_buf[50];
    		int uart_buf_len;
      /* USER CODE END 1 */
    
      /* MCU Configuration--------------------------------------------------------*/
    
      /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
      HAL_Init();
    
      /* USER CODE BEGIN Init */
    
      /* USER CODE END Init */
    
      /* Configure the system clock */
      SystemClock_Config();
    
      /* USER CODE BEGIN SysInit */
    
      /* USER CODE END SysInit */
    
      /* Initialize all configured peripherals */
      MX_GPIO_Init();
      MX_I2C1_Init();
      MX_TIM1_Init();
      MX_USART1_UART_Init();
      /* USER CODE BEGIN 2 */
      HAL_TIM_Base_Start(&htim1);
      delayUS(10000);
    
      	CommandSubcommands(BQ769x2_RESET);  // Resets the BQ769x2 registers
      	delayUS(60000);
      	BQ769x2_Init();  // Configure all of the BQ769x2 register settings
      	delayUS(10000);
      	CommandSubcommands(FET_ENABLE); // Enable the CHG and DSG FETs
      	delayUS(10000);
      	 CommandSubcommands(SLEEP_DISABLE); // Sleep mode is enabled by default. For this example, Sleep is disabled to
      									   // demonstrate full-speed measurements in Normal mode.
    
      	delayUS(60000);
      	delayUS(60000);
      	delayUS(60000);
      	delayUS(60000);  //wait to start measurements after FETs close
    
    
    
    
    
    
    
      /* USER CODE END 2 */
    
      /* Infinite loop */
      /* USER CODE BEGIN WHILE */
      while (1)
      {
    
        /* USER CODE END WHILE */
    
    
    
    	  Temperature[0] = BQ769x2_ReadTemperature(TS1Temperature);
    			uart_buf_len = sprintf(uart_buf, "%f : mV\r\n", Temperature[0]);            //
    			HAL_UART_Transmit(&huart1, (uint8_t *)uart_buf, uart_buf_len, 100);      //
    		//	delayUS(100000);
    		//	AlarmBits =0X01;
    		if (AlarmBits & 0x80) {  // Check if FULLSCAN is complete. If set, new measurements are available
        		BQ769x2_ReadAllVoltages();
        		Pack_Current = BQ769x2_ReadCurrent();
        		Temperature[0] = BQ769x2_ReadTemperature(TS1Temperature);
        		Temperature[1] = BQ769x2_ReadTemperature(TS3Temperature);
    			DirectCommands(AlarmStatus, 0x0080, W);  // Clear the FULLSCAN bit
    		}
    
    		if (AlarmBits & 0xC000) {  // If Safety Status bits are showing in AlarmStatus register
    			BQ769x2_ReadSafetyStatus(); // Read the Safety Status registers to find which protections have triggered
    			if (ProtectionsTriggered & 1) {
    				//HAL_GPIO_WritePin(GPIOA, LD2_Pin, GPIO_PIN_SET); }// Turn on the LED to indicate Protection has triggered
    				DirectCommands(AlarmStatus, 0xF800, W); // Clear the Safety Status Alarm bits.
    			}
    		else
    		{
    			if (ProtectionsTriggered & 1) {
    				BQ769x2_ReadSafetyStatus();
    				if (!(ProtectionsTriggered & 1))
    				{
    					//HAL_GPIO_WritePin(GPIOA, LD2_Pin, GPIO_PIN_RESET);
    				}
    			} // Turn off the LED if Safety Status has cleared which means the protection condition is no longer present
    		}
    		delayUS(20000);  // repeat loop every 20 ms
        /* USER CODE BEGIN 3 */
      }
      /* USER CODE END 3 */
    }
    
    }
    /**
      * @brief System Clock Configuration
      * @retval None
      */
    void SystemClock_Config(void)
    {
      RCC_OscInitTypeDef RCC_OscInitStruct = {0};
      RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
      /** Initializes the RCC Oscillators according to the specified parameters
      * in the RCC_OscInitTypeDef structure.
      */
      RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
      RCC_OscInitStruct.HSIState = RCC_HSI_ON;
      RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
      RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
      if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
      {
        Error_Handler();
      }
      /** Initializes the CPU, AHB and APB buses clocks
      */
      RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                                  |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
      RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
      RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
      RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
      RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
    
      if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
      {
        Error_Handler();
      }
    }
    
    /**
      * @brief I2C1 Initialization Function
      * @param None
      * @retval None
      */
    static void MX_I2C1_Init(void)
    {
    
      /* USER CODE BEGIN I2C1_Init 0 */
    
      /* USER CODE END I2C1_Init 0 */
    
      /* USER CODE BEGIN I2C1_Init 1 */
    
      /* USER CODE END I2C1_Init 1 */
      hi2c1.Instance = I2C1;
      hi2c1.Init.ClockSpeed = 400000;
      hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
      hi2c1.Init.OwnAddress1 = 0;
      hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
      hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
      hi2c1.Init.OwnAddress2 = 0;
      hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
      hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_ENABLE;
      if (HAL_I2C_Init(&hi2c1) != HAL_OK)
      {
        Error_Handler();
      }
      /* USER CODE BEGIN I2C1_Init 2 */
    
      /* USER CODE END I2C1_Init 2 */
    
    }
    
    /**
      * @brief TIM1 Initialization Function
      * @param None
      * @retval None
      */
    static void MX_TIM1_Init(void)
    {
    
      /* USER CODE BEGIN TIM1_Init 0 */
    
      /* USER CODE END TIM1_Init 0 */
    
      TIM_ClockConfigTypeDef sClockSourceConfig = {0};
      TIM_MasterConfigTypeDef sMasterConfig = {0};
    
      /* USER CODE BEGIN TIM1_Init 1 */
    
      /* USER CODE END TIM1_Init 1 */
      htim1.Instance = TIM1;
      htim1.Init.Prescaler = 0;
      htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
      htim1.Init.Period = 65535;
      htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
      htim1.Init.RepetitionCounter = 0;
      htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
      if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
      {
        Error_Handler();
      }
      sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
      if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
      {
        Error_Handler();
      }
      sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
      sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
      if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
      {
        Error_Handler();
      }
      /* USER CODE BEGIN TIM1_Init 2 */
    
      /* USER CODE END TIM1_Init 2 */
    
    }
    
    /**
      * @brief USART1 Initialization Function
      * @param None
      * @retval None
      */
    static void MX_USART1_UART_Init(void)
    {
    
      /* USER CODE BEGIN USART1_Init 0 */
    
      /* USER CODE END USART1_Init 0 */
    
      /* USER CODE BEGIN USART1_Init 1 */
    
      /* USER CODE END USART1_Init 1 */
      huart1.Instance = USART1;
      huart1.Init.BaudRate = 115200;
      huart1.Init.WordLength = UART_WORDLENGTH_8B;
      huart1.Init.StopBits = UART_STOPBITS_1;
      huart1.Init.Parity = UART_PARITY_NONE;
      huart1.Init.Mode = UART_MODE_TX_RX;
      huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
      huart1.Init.OverSampling = UART_OVERSAMPLING_16;
      if (HAL_UART_Init(&huart1) != HAL_OK)
      {
        Error_Handler();
      }
      /* USER CODE BEGIN USART1_Init 2 */
    
      /* USER CODE END USART1_Init 2 */
    
    }
    
    /**
      * @brief GPIO Initialization Function
      * @param None
      * @retval None
      */
    static void MX_GPIO_Init(void)
    {
      GPIO_InitTypeDef GPIO_InitStruct = {0};
    
      /* GPIO Ports Clock Enable */
      __HAL_RCC_GPIOC_CLK_ENABLE();
      __HAL_RCC_GPIOA_CLK_ENABLE();
      __HAL_RCC_GPIOB_CLK_ENABLE();
    
      /*Configure GPIO pin Output Level */
      HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13, GPIO_PIN_RESET);
    
      /*Configure GPIO pin : PC13 */
      GPIO_InitStruct.Pin = GPIO_PIN_13;
      GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
      GPIO_InitStruct.Pull = GPIO_NOPULL;
      GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
      HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
    
    }
    
    /* USER CODE BEGIN 4 */
    
    /* USER CODE END 4 */
    
    /**
      * @brief  This function is executed in case of error occurrence.
      * @retval None
      */
    void Error_Handler(void)
    {
      /* USER CODE BEGIN Error_Handler_Debug */
      /* User can add his own implementation to report the HAL error return state */
      __disable_irq();
      while (1)
      {
      }
      /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef  USE_FULL_ASSERT
    /**
      * @brief  Reports the name of the source file and the source line number
      *         where the assert_param error has occurred.
      * @param  file: pointer to the source file name
      * @param  line: assert_param error line source number
      * @retval None
      */
    void assert_failed(uint8_t *file, uint32_t line)
    {
      /* USER CODE BEGIN 6 */
      /* User can add his own implementation to report the file name and line number,
         ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
      /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */
    
    /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Arjun:

    可通过此链接找到 BQ769x2系列的所有微控制器示例代码: https://www.ti.com/lit/zip/sluc701。此外、TI 还提供有关如何对 BQ769x2器件系列进行编程的视频、网址为: https://www.ti.com/video/6270522957001。

    当您在 TI 的网站上提及这两组代码时、您是在谈论 BQStudio 还是其他内容? 如果是、值得注意的是 BQStudio 是被设计成与 SMBus 兼容的电路板一起使用的。 您能否共享原理图?

    此致!

    A·内德尔费尔德

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,先生,  

    没有 SIR 没有看到 BQSTUDIO 在这种情况下,我附上了我的原理图为您的 REF ..  似乎有 接地问题,请让我回答正确,

    e2e.ti.com/.../4743.Schematic-_2800_1_2900_.pdf

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    很抱歉、我附上了错误的原理图。

    低于 ACCTUAL 1

    e2e.ti.com/.../SS16_5F00_V2.0-14_2D00_06_2D00_2023-_2800_6_2900_.pdf

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、先生!

    我终于读写了新代码,  

    除此之外、我还有几个问题  

    1) 按照 TEC。 BQXXXX 数据表,我们可以使用100Khz 和400KHZ 的 I2C ,如果我想把 BQ I2C 设置为200Khz 可以吗?

    2)正如你刚才所说,在 BQ CRC 是 BYDEFAULT 启用那么,如果我想禁用相同的,我可以做同样的?

    3)在代码中,我想读的 CUV 和 COV 数据  ,我坐在这(  BQ769x2_SetRegister(COVThreshold, 0x55, 1 );) 到 VERYFIY 它是设置不是那么我怎么能做同样的?

    4) 4) 如何在进行 MICRCONTROLLER 编程后将 BQXXX 器件置于 SEALED 模式?

    5)直接命令和子命令和命令-子命令-以及我启用和禁用相同的 CRC ?

    感谢你先生的支持,我忠实地得到这些最后的问答.

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Arjun:

    1.该器件仅支持100kHz 和400kHz I2C。

    2.您需要修改 Settings:Configuration:Comm Type 中的寄存器以选择所需的通信模式。 我已在下面附上选项。 有关详细信息、请参阅 技术参考手册中的第9.1节

    3.如果您想查看是否发生了 COV 或 CUV,您可以读取 Safety Status A 寄存器位2和3中的值。 如果您想确定是否成功进行了写入、只需读取 Protections:CUV/COV:Threshold 下的 COV/CUV Threshold 寄存器。

    4.要将设备置于 SEALED 模式,可以设置 Security:Settings[SEAL]位,使其在上电时进入 SEALED 模式,也可以发送0x0030 SEAL()子命令将其置于 SEALED 模式。

    5.我无法完全确定您在这个问题上问了什么、但当您禁用 CRC 时、它也应该适用于命令和子命令。

    此致!

    A·内德尔费尔德

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,先生

    我想读取数据存储器,以验证写入所有 阈值后,我可以读取它们,我通过以下方式尝试相同的阅读 TEC 数据表 :-

    void BQ769x2_52 (Get_Register_)(uint16_t reg_add)
    {

    uint8_t RX_RegData[6]={0x00、0x00、0x00、0x00、0x00、 0x00};
    uint8_t rx_Byte[32]={0x00、0x00};

    uint8_t 长度;
    uint8_t crc_Rx;

    //TX_RegData、小端字节序格式
    RX_RegData[0]= reg_add 和0xff;
    RX_RegData[1]=(reg_add >> 8)和0xff;

    I2C_WriteReg (0x3E、RX_RegData、2);
    第36集7.3分庭(2000年);

    I2C_ReadReg (0x40、RX_34Byte、34);
    crc_rx = RX_34Byt[32];
    长度= RX_34Byte[33];

    for (int i =0;i<length;i++)
    {
    RX_34字节[i]= RX_34字节[40+i];

    但没有得到任何输出相同,请让我纠正我的错误,并作出更改。

     谢谢!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Arjun:

    当您说您遵循 TEC 数据表时、您是否参考了技术参考手册的第13.1节? 如果是、值得注意的是、它说在 x40处开始读取缓冲器。 我相信您的实施在以下行使用了40 (不是 x40):

    RX_34Byte[i]= RX_34Byte[40+i];

    不过值得注意的是、TI 确实提供了此函数、用于使用 BQ76952的 STM32读取寄存器:

    int I2C_ReadReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
    {
    	unsigned int RX_CRC_Fail = 0;  // reset to 0. If in CRC Mode and CRC fails, this will be incremented.
    	uint8_t RX_Buffer [MAX_BUFFER_SIZE] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    #if CRC_Mode
    	{
    		uint8_t crc_count = 0;
    		uint8_t ReceiveBuffer [10] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    		crc_count = count * 2;
    		unsigned int j;
    		unsigned int i;
    		unsigned char CRCc = 0;
    		uint8_t temp_crc_buffer [3];
    
    		HAL_I2C_Mem_Read(&hi2c1, DEV_ADDR, reg_addr, 1, ReceiveBuffer, crc_count, 1000);
    		uint8_t crc1stByteBuffer [4] = {0x10, reg_addr, 0x11, ReceiveBuffer[0]};
    		CRCc = CRC8(crc1stByteBuffer,4);
    		if (CRCc != ReceiveBuffer[1])
    		{
    			RX_CRC_Fail += 1;
    		}
    		RX_Buffer[0] = ReceiveBuffer[0];
    
    		j = 2;
    		for (i=1; i<count; i++)
    		{
    			RX_Buffer[i] = ReceiveBuffer[j];
    			temp_crc_buffer[0] = ReceiveBuffer[j];
    			j = j + 1;
    			CRCc = CRC8(temp_crc_buffer,1);
    			if (CRCc != ReceiveBuffer[j])
    				RX_CRC_Fail += 1;
    			j = j + 1;
    		}
    		CopyArray(RX_Buffer, reg_data, crc_count);
    	}
    #else
    	HAL_I2C_Mem_Read(&hi2c1, DEV_ADDR, reg_addr, 1, reg_data, count, 1000);
    #endif
    	return 0;
    }

    希望这对您有所帮助!

    此致!

    A·内德尔费尔德

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的先生,感谢您的谦虚支持。

    只是我想知道一个更多,因为我验证哪一个参数 我能够读取正确或不正确 ,然后我发现,一些参数我能够读取和写入正确,但有些不正确,有什么我不能理解? 或具有相同的任何具体原因? 请告诉我!  

    因为我知道 delay 是两个字节,也有写入_set_Bq_register() 但仍然没有得到实际值,这是我设置的

    ~Arjuna

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Arjun:

    你能不能去读一本书吗? Protections:OCC:Recovery Threshold 或任何其他两字节参数、以确定问题是否与两字节寄存器有关? 如果 SET_bq_register ()函数与 TI 提供的 I2C_WriteReg ()函数不同、您是否也可以共享该函数?

    另外、您是否已确认这是否完全是读取错误而不是写入错误? 通过测试触发 COV 所需的时间来确保使用示波器完成写入可能是一种明智的做法。 写入之前的延迟应该为~244.2ms。 当您尝试读取延迟值时、您能否展示逻辑分析仪对发送和接收的波形的捕获? 这还将深入了解读取/写入错误的位置。

    此致!

    A·内德尔费尔德

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、先生、由于我的上述问题已经解决、

    现在,我在同一 IC (BQ7695202 )又面临一个问题,在这一次,我将使用 BQstudio 编程我的 BMS(英语:BQ7695202)。 (我有2个 BMS、电流为40安培、电流为60安培)  

    当我对40安培的 BMS 进行短路时、SCD 工作正常。

    但是当我 用60安培的 BMS 进行短路时,  然后 BQ76xxx 反复复位(看门狗定时器位变高)并通过执行同样的7-8次、BQ7xx 变为关断模式(如 BQ 技术数据表中所述-由于 RAM 故障发生 )

    我们已经验证了所有内容并尝试了可能的解决方案、但无法获得相同的解决方案、

    请让您给我同样的解决方案、这对我们来说非常重要。

    我已经随附了 BMS 的原理图以及两个(40/60安培)的.gg 文件

    e2e.ti.com/.../SLERU16040V0200R1_5F00_DT255.gg-_2800_1_2900_.csv

    e2e.ti.com/.../SS16_5F00_V2.0-14_2D00_06_2D00_2023-_2800_8_2900_.pdf

    e2e.ti.com/.../SS16_5F00_13022023.gg.csv

    这是我们在 SCD 期间得到的结果。

    除此之外、我还看到、在短路放电期间、BQ7xx 变得略微变热、并进入内部温度过高故障状态。 在该 BQxx 再次复位之后(WD 位始终变为高电平)。

    问题2. 我的最后一个问题是、剂量 BQ76952内核使用卡尔曼滤波器估算准确的 SoC、如果不是、那么我们获得的 SoC 是准确的、我如何理解这个概念、或者如果您有与该概念相关的文档、请分享。

    谢谢。此

    致、
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Arjun:

    在查看您的.gg 文件时、我不确定您当前的计算是正确的。 40A 和60A 的相应 SCD 阈值为7和10。 如果您的电流检测电阻器设置为8个并联的电阻器、则得出的总电阻为1.25m Ω。 SCD 阈值为7意味着 SRP 和 SRN 引脚之间总共看到150mV 的电压。 现在如果有电阻、您需要大约120A 来触发 OCD、而不是40A。 同样、10表示 SRP 和 SRN 引脚上的电压为250mV、与触发所需的200A 电流相关。

    您能否确认器件在短路事件期间达到200A? 否则不会触发故障、从而使器件在电池组电压随着短路下降而断电。 如果电量不足、如果内存不再能通电、可能会发生 RAM 故障。

    对于第二个问题、该芯片没有内置卡尔曼滤波器来确定 SoC。 不过、该器件可提供确定 SoC 所需的所有电压、电荷和电流。 如果您愿意、可以将 BQ34Z100-G1等堆栈级别测量仪表与 BQ769x2结合使用来提供 SoC 计算。

    此致!
    A·内德尔费尔德

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、先生!

    抱歉、我忘了提一下这些问题:-

    对于60A --> 分流器10毫欧(8个) = REQ = 1.25毫欧

    对于40A -->分流器4毫欧(4个) = REQ = 1毫欧

    at .gg 文件

    对于60A  --> SCD = 10 (250mV) = 200A

    对于40A  --> SCD = 7 (150mV) = 150A

    还有一点是、在短路放电期间、 由于 I2C 连接丢失1-2秒、BQ76952完全复位并且 REG1电压变为零、然后 BQ7xx 被吸入环路中且看门狗位变为高电平-永远

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Arjun:

    运行60A SCD 测试时是否会触发 SCD? 器件在一次短路中不会发热太多、尤其是在室温~30C 的情况下。 您是否曾尝试交换 BQ769x2芯片以查看是否在多个器件上仍然存在相同的问题?

    完全复位是清除所有寄存器还是刚刚重新启动硬件? 一般情况下、如果 SCD 未触发、而器件继续拉高电流、电池组电压下降、芯片可能会停止供电。

    我将在早上尝试运行您的.gg 文件、以查看是否可以在 EVM 上看到相同的结果。

    此致!
    A·内德尔费尔德

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、先生!

    1.是的、SCD 被触发并尝试了不同的 BQ76x2器件、但发生了相同的问题。

    2、它只是因为 I2C 连接丢失,我们在相同 OTP 之后所做的更改 也由于 REG1上的电源丢失而被重置  

    好,先生,让我知道背后的原因是什么!  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Arjun:

    除了检测电阻变化外、该设置的硬件是否有任何变化? 在 EVM 上测试.gg 文件时、我能够触发 SCD、并关闭 FET。

    最好检查的一件事是您的所有 DSG FET 仍处于良好状态。 FET 可能以某种方式损坏并充当短路、因此无论 DSG FET 是否导通、电流均可流动。 如果是这种情况、短路触发 SCD 是软件将无法关闭栅极。 这将导致芯片无法加电、从而导致复位。

    同样、您在使用什么进行 SCD 测试? 通常、最好使用没有电流限制的电池、如电源、以确保可以达到200A。 我注意到您的延迟是~450uA、因此如果您尝试使用电源进行测试、则最好尝试缩短延时时间。 这可能不会修复任何问题、但可以进行测试。

    最后一个问题、为什么您在电源路径上的 FET 栅极与源极之间改变电阻? 典型应用使用10M Ω 电阻器、但您似乎同时使用了1M Ω 和470K 电阻器。

    此致!
    A·内德尔费尔德